Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

How do I install the software for the X8711A IoT Device Functional Test Solution?

It is recommended to use the installation wizard to install the software components. The installation wizard can be found at keysight.com/find/X8711A under Technical Support then the Drivers, Firmware & Software tab. There is both an on-line and off-line installation download available.

If there is a need to manually install the software components, refer to the instructions.
 

Ссылки, относящиеся к этой теме