Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

33521A and 33522A Function / Arbitrary Waveform Generator Videos

Lowest jitter and total harmonic distortion in its class

33521A/33522A Image

The 33521A and 33522A Function/Arbitrary Waveform Generators provide you with 30 MHz bandwidth, one or two channels, 16-bits of vertical resolution, excellent pulse capabilities, and a variety of other useful features.

  • For a quick 3.5-minute product demonstration, view the "product overview" video below.
  • View the “how to” videos for more details on individual product features.

The 33500 Series video demos require Windows® Media Player. You may download and install the player from the Windows Media Player home page. 

Документы и файлы для загрузки

33521A & 33522A Video: Product Overview 
3.5-minute video illustrates the unique capabilities of the 33521A/22A function / arbitrary waveform generators. With 30 MHz bandwidth & flexible arbitrary waveform capabilities these generators set a new standard for performance & value. (3:29 mins)

Демонстрация 2010-08-01

33521A & 33522A Video: How to Sum Two Signals on a Single Channel 
See how to create a 2-tone telecom signal using one channel and the SUM capability of the 33521A/22A function / arbitrary waveform generators. The video also shows how to add white noise to a waveform using only one channel. (2:16 mins)

Демонстрация 2010-08-01

33521A & 33522A Video: How to Vary Pulse Edge Times and Set Up Pulse Width Modulation 
See how to generate pulses and adjust rise and fall times independently on the 33521A/22A function / arbitrary waveform generators. The video also demonstrates how to set up and use Pulse Width Modulation (PWM.) (1:31 mins)

Демонстрация 2010-08-01

33521A & 33522A Video: How to set up Pseudo Random Bit Streams (PRBS) 
See how to use the unique Pseudo Random Bit Stream (PRBS) waveform generation capability of the 33521A/22A function / arbitrary waveform generators. These waveforms are especially useful for testing communication devices. (2:02 mins)

Демонстрация 2010-08-01

33521A & 33522A Video: How to Synchronize and Adjust Phase between Two Channels 
See how to set up two channels and synchronize their phase. Additionally, you can adjust the phase between the two signals. (1:13 mins)

Демонстрация 2010-08-01

33521A & 33522A Video: How to set up Sweep, Dwell Time, Return Time and Create Frequency Lists 
See how to use some of the unique sweep features of the 33521A/22A function / arbitrary waveform generators. In addition to selecting start freq., stop freq. and sweep time, you can also set dwell time, return time and sweep freq. lists. (1:36 mins)

Демонстрация 2010-08-01

33521A & 33522A Video: How to Use Tracking to Create Differential Signals 
See how to lock two channels together so that they track each other exactly in phase and amplitude. By then using the capability to invert one of the channels, you can generate differential outputs. (1:38 mins)

Демонстрация 2010-08-01

33521A & 33522A Video: How to Couple 2 Channels in Frequency and/or Amplitude, with Ratio & Offset 
See how to create two independent outputs and then couple them in amplitude and/or frequency, either by fixed frequency ratio or fixed offset frequency. (1:56 mins)

Демонстрация 2010-08-01

33521A & 33522A Video: How to Use Variable Bandwidth Noise 
See how to reduce the bandwidth of the 30 MHz white noise output, thereby limiting the frequency and increasing the amplitude of the white noise energy into your device under test. (1:14 mins)

Демонстрация 2010-08-01

33521A & 33522A Video: How to Use the Front Panel Controls 
See how to select different waveforms, set their parameters and adjust units such as voltage and frequency using soft keys and the numeric keypad or knob. Also see how to invoke sweep, burst and modulation. (2:22 mins)

Демонстрация 2010-08-01

33521A & 33522A Video: How to Edit a Waveform Using the Waveform Editor 
See how to edit a waveform stored in the 33521A/22A function / arbitrary waveform generator using the internal waveform editor capabilities. (1:37 mins)

Демонстрация 2010-08-01

33521A & 33522A Video: How to Capture a Scope Waveform and Download it to the Function/ARB Generator 
See how to capture a waveform from a scope, transfer it to the arbitrary generator via a USB Flash drive, and output the waveform from the generator, all in less than 40 seconds! (1:21 mins)

Демонстрация 2010-08-01

33521A & 33522A Video: How to Create ARB Waveforms Using the Built-in Waveform Editor 
See how to use the embedded waveform editor to create a damped sine wave, using built-in functions and math. (2:00 mins)

Демонстрация 2010-08-01

33521A & 33522A Video: How to Sequence Arbitrary Waveforms 
See how to generate a sequence of up to 512 arbitrary waveforms per channel. Individual arbitrary waveforms can be combined into sequences to form longer, more complex waveforms. (2:05 mins)

Демонстрация 2010-08-01