Can I upgrade my Windows® XP logic analyzer to Windows Vista?
Version 3.80.0002 of the Agilent Logic Analyzer application has added support for Windows ®Vista. However, as of February 2009, Vista should not be installed on any 1680/16800/16900-series logic analyzers. This is because Agilent has not yet implemented the hardware cooperation required for operation under Vista.
Agilent Logic Analyzer can be installed on a PC running Windows Vista, as either an offline viewer or for control of logic analyzer hardware via LAN (i.e. hosted mode).
The latest version of Agilent Logic Analyzer is available at: http://www.agilent.com/find/16900_sw_download
Windows is a U. S. registered trademark of the Microsoft Corporation.