Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

How can I clear an error message shown on the display of the 4294A/4395A/4396B by using GPIB command?

Send the "KEY 18" command to the instrument.

Sending this command is equal to pressing the "Entry Off" key on the front panel, which clears the error message on the display of the instrument. The details about KEY command are described in the manual of each instrument;

4294A Precision Impedance Analyzer Programming Manual (page 323)

4395A Network/Spectrum/Impedance Analyzer Programming Manual (page K-1)

4396B Network/Spectrum/Impedance Analyzer GPIB Command Reference (page 2-55)