Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Is there an example program for acquiring Keysight ESA Series Spectrum Analyzer Family Trace Data via GPIB, VEE, and the REAL 32 bit data format command?

Yes. The attached pdf file explains a program that executes the 32 bit real acquisition from the Agilent ESA. The program was developed in VEE graphical programming language. The programming concepts can be used with most other programming languages. VEE users can download the attached Vee development program.