Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

1653xA: I would like to be able to do high frequency rejection to filter a signal captured by the 16534A. Is that possible?

Unfortunately, the 16534A does not have that capability. The only way around this, is to filter the signal prior to the scope input.

Revision 1.0 17 NOV 99 ahd