Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

What is the internal Arb trigger delay jitter?

The internal Arb trigger delay is generated using a free running oscillator. Using any delay other than zero guarantees jitter.

A firmware fix is available in C.04.60 (ESG) and C.04.61 (PSG) that allows the delay to be specified in time or in clock samples. When the delay is specified in clock samples the delay is synchronized to the Arb sample clock. This eliminates the jitter introduced by the free running oscillator.