Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

How do I update the operating system in an N9038A MXE EMI receiver from Windows XP to Windows 7?

The Windows 7 operating system (Windows Embedded Standard 7) that is now used in all new MXEs is a 64-bit operating system, while the Windows XP operating system previously used was a 32-bit operating system. Also, the processor assemblies that were used in all MXEs with the Windows XP operating system contain a 32-bit processor. So all operating system updates will require an upgrade of the processor assembly to the new 64-bit processor assembly.

For information on what an operating system update will require for an MXE please see Option W7X on the How do I upgrade my N9038A MXE EMI Receiver page.