이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

How do I upgrade my N9048B PXE EMI Receiver?


Most all of the N9048B options that are sold at the time of instrument purchase are also available as an upgrade option. The upgrades are either Software Licensed Options or Measurement Applications. The upgrade contents are described in the tables below as License Key. Kits will contain the installation instructions. A license key will be required to activate the hardware option or measurement application. Upgrade options are categorized as:

  • Internal Hardware Upgrades (Ex. PFR, YAS)
  • Instrument Software (Ex. Instrument Software & Measurement Applications, SF1)

Internal Hardware Upgrades:

Before a hardware upgrade is purchased the following steps should be taken:

  1. View the installation instructions by selecting the "Available" links in the tables below for the desired upgrade option.
  2. Determine from the installation instructions the complexity of the installation and whether you will perform the upgrade yourself or have a Keysight Service Center do it for you.

X-Series Performance Verification Tests  

If an upgrade option is going to be installed by an Keysight Service Center, additional labor charges will apply. Your Keysight field engineer can provide an all inclusive quote for this.

All PXE upgrades will require the redemption and installation of a license key file (.lic) to activate the option. Once a redemption certificate is received the license key file can be redeemed at the Keysight Software License Redemption Website

N9048B Internal Hardware Option Upgrades
Option Description Order As eDelivery Installation Note Upgrade Contents Minimum Firmware Adjustments Required Additional Requirements Incompatible With Installed By Installation Time

B25

25 MHz Analysis Bandwidth N9048BU-B25 Yes Available License Key None No None None Advanced User Install=0.5 Hrs
Verify=0.5 Hrs
B40 40 MHz Analysis Bandwidth N9048BU-B40
 
Yes Available License Key None No None None Advanced User

Install=0.5 Hrs
Verify=0.5 Hrs

CR3 Connector, Wideband IF Output N9048BU-CR3
 
Yes Available License Key None No None None Advanced User

Install=0.5 Hrs
Verify=0.5 Hrs

P03 Preamplifier, 3.6 GHz N9048BU-P03 Yes Available License Key None No None None Advanced User

Install=0.5 Hrs
Verify=0.5 Hrs

P08 Preamplifier, 8.4 GHz N9048BU-P08 Yes Available License Key None No None None Advanced User

Install=0.5 Hrs
Verify=0.5 Hrs

P26 Preamplifier, 26.5 GHz N9048BU-P26 Yes Available License Key None No None None

Advanced User

Install=0.5 Hrs
Verify=0.5 Hrs

PFR Precision frequency reference N9048BU-PFR Yes Available License Key None No None None Advanced User

Install=0.5 Hrs
Verify=0.5 Hrs

SF1 Security Feature, Exclude Launching Programs N9048BU-SF1 Yes Available License Key None No None None Advanced User

Install=0.5 Hrs
Verify=0.5 Hrs
 

SF2 Security Feature, Prohibit Saving Results N9048BU-SF2 Yes Available License Key None No None None Advanced User Install=0.5 Hrs Verify=0.5 Hrs
SS1 Additional removable solid state drive, Win10 N9048BU-SS1 Yes Available License Key None No None None Advanced User Install=0.5 Hrs
Verify=0.5 Hrs.
YAS Y-axis screen video output N9048BU-YAS Yes Available License Key None No None None Advanced User

Install=0.5 Hrs
Verify=0.5 Hrs

Instrument Measurement Software

Instrument Software Updates:

The software update package for the PXE EMI Receiver contains the Spectrum Analyzer measurement application, the EMI Receiver measurement application, all the advanced measurement application software, and all other updates required by the individual measurement assemblies inside the instrument.
Keysight recommends updating the instrument software version whenever an internal hardware upgrade or measurement application is installed into the instrument.
 

Measurement Applications:
 

The following is a list of the currently available optional measurement applications for the M9048A EMI Receiver:
 

 

To install an optional measurement application the purchase of a valid redemption certificate is required.
 

Measurement application upgrades are meant to be performed by the user, and no adjustments or performance verification testing is required.
 

문서자료 및 다운로드

내 스펙트럼/신호 분석기를 업그레이드하려면 어떻게 해야 합니까?  
스펙트럼 분석기 업그레이드 또는 신호 분석기 업그레이드를 수행하기 위한 정보.

고객문의 2019-04-30