이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

Do all Power Products ship with a calibration certificate?

Criteria have been established to determine which products get or do not get a calibration from the factory. A product with a product number does not automatically qualify for a calibration certificate.

Products which meet the following 3 criteria will ship with a calibration certificate:

1. The product must have published specifications.

2. The product must be calibrated: specifications are checked and metrology is in place.

3. There is a likelihood the product will be recalibrated in the field at the recommended calibration intervals to qualify for a calibration certificate.

Currently, four Power Products that are not shipped with a calibration certificate are the 6050A, 6051A, 66000A and N3300A. Each of these is a mainframe power unit which houses separate plug-in modules. There are no specifications to be checked on these products, and they do not have a recommended calibration interval in the field. Therefore, there is no need for a calibration certificate for these products.