이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

What are the units used when setting the current slew rate in the electronic loads from the front panel and over the GPIB?

For the N3300A series electronic loads, all slew rate entries from the front panel or over the GPIB are done in the units of amperes per second (A/s).

For the 6060B, 6063B and mainframes 6050A and 6051A with load modules, the slew rates units are entered from the front panel in amperes per microsecond (A/us) and over the GPIB in amperes per second (A/s).