이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

When powered on, what is the wake-up voltage and current setting of the 606xB and 6050xB Series electronic loads?

The 606xB and 6050xB Series have 7 user-definable recall states which allow saving the settings of the load for later recall. One of these states, location 0 is non-volatile; this is called the wake-up state. The 606xB and 6050xB will be set to the state stored in location 0 at power turn-on. If no state has been saved to location 0, then it will still contain the factory-default state. The factory default state normally would be 0 V and 0 A. See *SAV in Programming Manual 06060-90005.