検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

I want to use multiple 2-port M9371A PXIe VNAs in my system. Is option 551 necessary?

If the modules are used as independent 2-port VNAs, no; however, option 551 is necessary to perform true, calibrated, multiport measurements.

See page 15 of the configuration guide for example configurations:

     PXI Vector Network Analyzer - Configuration Guide