Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

What is the difference between EVM1, EVM10 and Peak EVM when using the Keysight 8920B?

There are three different EVM measurements available with the Agilent 8920B Option 80X:

  • EVM1 - rms average EVM of one entire burst (standards specify rms).
  • Peak EVM - peak EVM of one entire burst.
  • EVM10 - rms average EVM of first 10 symbols of 10 bursts.

(c) Copyright Agilent Technologies 1999, 2000.

This information is subject to change without notice and is provided "as is" with no warranty. Agilent Technologies shall not be liable for any direct, indirect, special, incidental or consequential damages in connection with the use of this material.