Here’s the page we think you wanted. See search results instead:

 

Discutez avec un expert

What is the performance difference between the N8212A module with Option 016 and the N8241A arbitrary waveform generator synthetic instrument module?

The N8212A with Option 016 is a synthetic instrument based on the E8267D PSG signal generator with Option H16. It does not have a display or an internal Arb.

The N8241A is a synthetic instrument based on the N6030A arbitrary waveform generator. Communication with the N8241A is made through LAN, not an NI interface.