Here’s the page we think you wanted. See search results instead:

 

Discutez avec un expert

How do I access the A32 memeory space of VXI through an E1406A?

Situation:

The E1406A cannot access the A32 memory space of VXI. It is also limited, as permitted by the VXI specification, to only accessing the 0x200000 to 0xDFFFFF portion of A24 space.

Solution:

If A32 access or additional A24 range is required, consider using an embedded controller, MXI, or the E8491B VXI-Firewire interface.