Here’s the page we think you wanted. See search results instead:

 

Sprechen Sie mit einem Experten

N9000B CXA Signal Analyzer Upgrades

Most all of the N9000B options that are sold at the time of instrument purchase are also available as an upgrade option.  Upgrade options can vary from a simple license key installation to more complex upgrades that involve installling multiple pieces of hardware. For each upgrade option it is advised that each row in the table is read and understood. Before purchasing an upgrade option that contains hardware items, the following steps should be taken:
 

  1. View the installation note by selecting the Install Note link in the Upgrade Contents cell. 
  2. Determine from the installation instructions the complexity of the installation and whether you will perform the upgrade yourself or have a Keysight Service Center perform the installation. 
  3. Review the Utilities, Adjustments & Performance Verification Tests section of the installation instructions to see what the required adjustments and performance tests are once the upgrade is installed. 
  4. Review the following lists of test equipment requirements for each required adjustment and performance test to further determine whether you have the ability to perform the upgrade yourself or have an Keysight Service Center perform the installation.

If an upgrade option is going to be installed by a Keysight Service Center, additional labor charges may apply. Your Keysight field engineer can provide an all inclusive quote for this.

All instrument adjustments are automated and require the use of the Keysight Performance Verification & Adjustment Software.

Many hardware upgrades will require the redemption and installation of a license key file (.lic) to activate the option. Once a redemption certificate is received the license key file can be redeemed at the Keysight Software License Redemption Website

N9000B Internal Hardware Options
Option Description Order As eDelivery Upgrade Content Minimum Firmware Adjustments Required1 Additional Requirements Incompatible With Installed By Installation Time
B25

25 MHz Analysis Bandwidth
Bandwidth Upgrade Wizard

N9000BU-B25

Yes
  1. Install Note
  2. Entitlement Certificate
None No None None Service Center Recommended3

Install=0.5 Hrs
Adjust & Verify=0.5 Hrs

EDP Enhanced Display Package N9000BU-EDP Yes
  1. Install Note
  2. Entitlement Certificate
None No None None User Install=0.5 Hrs
Adjust & Verify=0.0 Hrs
EMC Basic Precompliance EMI Feature N9000BU-EMC Yes
  1. Install Note
  2. Entitlement Certificate
     
None No None None User Install=0.5 Hrs
Adjust & Verify=0.0 Hrs
ESC External Source Control Feature N9000BU-ESC Yes
  1. Install Note
  2. Entitlement Certificate
  3. Hardware
     
None No None 513, 526 User Install=0.5 Hrs
Adjust & Verify=0.0 Hrs
FSA Fine Resolution Step Attenuator N9000BU-FSA Yes
  1. Install Note
  2. Entitlement Certificate
     
None Yes None None Service Center Recommended3

Install=0.5 Hrs
Adjust & Verify=3.0 Hrs

P03 Preamplifier, 3 GHz N9000BU-P03 Yes
  1. Install Note
  2. Entitlement Certificate
     
None Yes None P07, P13, P26 Service Center Recommended3

Install=0.5 Hrs
Adjust & Verify=2.5 Hrs

P07 Preamplifier, 7.5 GHz N9000BU-P07 Yes
  1. Install Note
  2. Entitlement Certificate
     
None Yes None 503, P13, P26 Service Center Recommended3

Install=0.5 Hrs
Adjust & Verify=2.5 Hrs

P13 Preamplifier, 13.6 GHz N9000BU-P13 Yes
  1. Install Note
  2. Entitlement Certificate
     
None Yes None 503, 507, P26 Service Center Recommended3

Install=0.5 Hrs
Adjust & Verify=2.5 Hrs

P26 Preamplifier, 26.5 GHz N9000BU-P26 Yes
  1. Install Note
  2. Entitlement Certificate
     
None Yes None 503, 507, 513 Service Center Recommended3

Install=0.5 Hrs
Adjust & Verify=2.5 Hrs

PFR Precision Frequency Reference N9000BU-PFR Yes
  1. Install Note
  2. Entitlement Certificate
     
None Yes None None Service Center Recommended3

Install=0.5 Hrs
Adjust & Verify=1.0 Hr

SF1 Security Features, Exclude Launching Programs N9000BU-SF1 Yes
  1. Install Note
  2. Entitlement Certificate
     
None No None None User Install=0.5 Hrs
Adjust & Verify=0.0 Hrs
SF2 Security Features, Prohibit Saving Results N9000BU-SF2 No
  1. Install Note
  2. Entitlement Certificate
     
None No None None Service Center Recommended Install=1.0 Hrs
Adjust & Verify=0.0 Hrs
SSD Windows Embedded Standard 7 Solid State Drive ⇒ MUST READ N9000BU-SSD No
  1. Hardware
  2. Install Note
  3. Software
None No2 None None Service Center Recommended Install=0.5 Hrs
Adjust & Verify=0.5 Hrs
T03 Tracking Generator, 3 GHz N9000BU-T03 No
  1. Hardware, License Key
  2. Install Note
None Yes None None Service Center Recommended Install=1.0 Hrs
Adjust & Verify=2.0 Hrs
 
T06 Tracking Generator, 6 GHz N9000BU-T06 No
  1. Hardware, License Key
  2. Install Note
None Yes None None Service Center Recommended Install=1.0 Hrs
Adjust & Verify=2.0 Hrs
 
W10 Windows 10 Solid State Drive ⇒MUST READ N9000BU-SS1 No
  1. Hardware
  2. Install Note
  3. Software
None No2 PC7 None Advanced User Install=1.0 Hrs
Adjust & Verify=0.0 Hrs
 

 

N9000B External Hardware Options
Option Description Order As eDelivery Upgrade Content Minimum Firmware Adjustments Required1 Additional Requirements Incompatible With Installed By Installation Time
1CM113A Rackmount Kit (Rack Flanges Only) 1CM113A No
  1. Hardware
  2. Install Note
None No None PRC, 1CN103A, 1CP105A User Install=0.5 Hrs
1CN103A Front Handle Kit (Handles Only) 1CN103A No
  1. Hardware
  2. Install Note
None No None PRC, 1CM113A, 1CP105A User Install=0.5 Hrs
1CP105A Rack Mount Kit with Handles 1CP105A No
  1. Hardware
  2. Install Note
None No None PRC, 1CM113A, 1CN103A User Install=0.5 Hrs
1CR013A Rack Slide Kit (Rack Slides Only) 1CR013A or E4406-60115 No
  1. Hardware
  2. Install Note
None No None PRC User Install=1.0 Hr
1DVR001A USB DVD-ROM/CD-R/RW Drive 1DVR001A or 0950-5369 No
  1. Hardware
None No None None Not applicable Not applicable
1KYB001A USB Keyboard - Compact 1KBD001A or 0960-2929 No
  1. Hardware
None No None None Not applicable Not applicable
MLP001A Minimum Loss Pad, 50-to-75 Ohms MLP001A or 0955-1020 No
  1. Hardware
None No None None Not applicable Not applicable
1MSE001A USB Mouse 1MSE001A or 0960-2670 No
  1. Hardware
None No None None Not applicable Not applicable
PRC Portable Configuration N9000BU-PRC
 
No
  1. Hardware
  2. Install Note
None No None 1CM113A, 1CN103A, 1CP105A, 1CR013A User Install=1.0 Hr

1 While the completion of the recommended adjustments and performance tests for a given option upgrade does verify the functionality of the option, it does not guarantee that the entire instrument meets all published specifications. A full instrument calibration is the only way to guarantee that all instrument specifications are being met.
2 The instrument calibration data file MUST be transferred in order for the analyzer to meet specifications. If the cal file is not transferred all adjustments and performance tests must be performed. Refer to the Installation Note for details.
Upgrade can be performed by the User without any performance verification required if the instrument being upgraded is still within it's original factory calibration cycle and no major repairs or adjustments have been performed on it. See the upgrade installation note for more details.

Instrument Software:

Instrument Software Update:

The software update package for the X-Series Signal Analyzers contains the spectrum analyzer measurement application, all the advanced measurement application software, and all other updates required by the individual measurement assemblies inside the instrument.

Keysight recommends updating the instrument software version whenever an internal hardware upgrade or measurement application is installed into the analyzer.

The latest revision of the instrument software installer can be found at:

Measurement Applications:

To see the complete list of software measurement applications available for the N9000B Signal Analyzer, see:

Measurement Applications require the redemption and installation of a license key file (.lic). Measurement application upgrades are meant to be performed by the customer, and no adjustments or performance verification tests are required.

In order to redeem a license key, the end user must have a valid redemption certificate and then go to the Keysight Software License Redemption Website.

Available Accessories:

Documents & Downloads

How do I upgrade my Spectrum / Signal Analyzer? 
Information to perform a spectrum analyzer upgrade or signal analyzer upgrade.

FAQ 2014-12-18