Here’s the page we think you wanted. See search results instead:

 

Sprechen Sie mit einem Experten

How do I configure my external video monitor output on the ENA?

(SUPPORTED MODELS IN BOLD: E5071C E5072A E5070B/71B E5070A/71A E5061A/62A E5061B E5063A E5091A E5092A)

In order to configure the video monitor output on the ENA, ensure you have chosen the "Intel Dual Display Twin" for the display mode, as noted in the following steps:

  1. Connect the external monitor to the video port of the ENA and power on the monitor.
  2. Access the Windows desktop of the ENA.
  3. Select START from within the windows desktop tool bar.
  4. Select Control Panel
  5. Choose the "Intel Graphics Technology" icon.
  6. Select "Intel Dual Display Twin" from the "Devices" and check "Activate Intel Dual Display Twin", then click "Apply" (refer to image below).

ENA-B Series Network Analyzer Screenshot

Important Note:
Due to hardware configuration differences the external video configuration information above is applicable to the ENA, which have a horizontal rear panel video connector. This process is not applicable to earlier versions of the ENA, which have a vertical video output connector.