这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

What are the benefits of the built-in VBA?

(SUPPORTED MODELS IN BOLD: E5071C E5072A E5070B/71B E5070A/71A E5061A/62A E5061B E5063A E5091A E5092A)

1. Built-in VBA on the ENA improves your network measurement environment.

The product note, "Evolution of Test Automation Using the built-in VBA with the ENA Series RF Network Analyzers", explains how the built-in VBA can improve your network measurement environment. Practical examples of the effective use of the built-in VBA are given in the product note. For more information

2. VBA program launcher (Firmware Revision 3.50 or later) allows you to enhance the ENA's capability with your own VBA programs.

You can select VBA program by pressing "Macro Setup" > "Load & Run".

3. VBA sample program library saves your development time.

The VBA sample program library provides various useful programs such as a filter measurement program, data saving utility, calibration wizard and more. By downloading sample programs, you can modify a sample program to meet your specific needs and save your development time compared to making programs from scratch.

For specific VBA sample programs for the ENA, visit the web links below:

E5071C

E5070B/71B

E5061A/62A

E5061B

E5072A

For additional ENA product information, visit the ENA Series of Network Anlayzers' Web page.