这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

Which 34980A Switch Modules are supported by the IviSwtch api?

The following modules are SUPPORTED by the IviSwtch API of the 34980A IVI driver:

  • 34921A
  • 34922A
  • 34923A
  • 34923A-1W
  • 34924A
  • 34925A
  • 34925A-1W
  • 34931A
  • 34932A
  • 34933A
  • 34933A-1W
  • 34934A-4x32
  • 34934A-4x64
  • 34934A-4x128
  • 34934A-8x32
  • 34934A-8x64
  • 34934A-16x32
  • 34937A
  • 34938A
  • 34939A
  • 34941A
  • 34942A
  • 34946A
  • 34947A

The following modules are NOT SUPPORTED by the IviSwtch API, but can be accessed using the Ag34980a specific driver:

  • 34945A
  • 34950A
  • 34951A
  • 34952A
  • 34959A

 

Last Revised: January 21, 2014 - driver version 1.5.3.0