这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

B2900A Program Examples included in B2900 Product Reference CD-ROM

Description

The sample folder contains sample programs for the Keysight B2900 series Precision Source/Measure Unit. Copy all of the sample programs to your hard disk before use.

There are three sweep measurement sample programs written in the following programming languages:

  • Microsoft® Visual C#® with VISA-COM
  • National Instruments LabVIEW with VISA-COM
  • Microsoft Excel with VISA-COM
     

Requirements

  • Microsoft Visual Studio® 2010
  • NI LabView 8.6.
  • Microsoft Excel 2007
  • Keysight I/O Library 16.0 or later

Microsoft, Visual C# and Visual Studio are trademark or registered trademarks of Microsoft Corporation in the United States and/or other countries.

文档和下载

B2900A Program Examples included in B2900 Product Reference CD-ROM 
The sample programs for the Keysight B2900 series Precision Source/Measure Unit including three sweep measurement sample programs written in the following programming languages, Microsoft® Visual C#®, Excel VBA and National Instruments LabVIEW.

编程实例 2011-06-01

null ZIP 270 KB