这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

What is the possible cause of the difference when the permittivity measured with the 16453A is different from the value previously obtained?

Most likely cause of the measurement discrepancy or drift is insufficient electrode pressure due to improper pressure adjustment. Set the pressure adjustment nut of the 16453A to the maximum pressure without deforming the dielectric material sample.