这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

Can the 16338A be used with LCR meters such as the 4263B and the E4980A?

No, the 16338A Test Lead Set doesn’t have compatibility with LCR meters. The 16338A can only be used with the 4338A/B because the measurement circuit operating principle of the 4338A/B is different from that of the LCR meters. The 16338A has been designed to operate specifically with the 4338A/B.