这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

When the 41800A Active Probe or the 41802A 1 MΩ Input Adapter is used with the 4395A, is any calculation required for converting the data at 1 MΩ input into that at 50 Ω input?

No, any conversion calculation related to the difference in input impedance (between 1 MΩs and 50 Ωs) is not required. You can directly read the measurement value on the 4395A.