这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

Windows login process appears on my ENA every time after power up. Can I skip this?

(SUPPORTED MODELS IN BOLD: E5071C E5070B/71B E5070A/71A E5061A/62A E5061B E5072A)

In default setting, windows login process does not appear and go directly to the NA application after power up.
Required conditions for this are:

  • Use welcome screen for login. (default = use welcome screen)
  • Only one user account is registered to windows. (default = only "agena" is registered)
  • ENA is not attending to a domain. (default = Member of workgroup)
  • Password is not active for the account. (default = no password)

Login process will appear if more than one of above setting is changed by user. If such user still requires bypassing windows login process, use windows auto login function:

  1. Click Start, click Run, and type "control userpasswords2".
  2. Uncheck the "Users must enter a username and password to use this computer" check box.
  3. Click Apply.
  4. Enter the user name and password you wish automatically log on with, and then click OK.
  5. Click OK again.