这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

What are the major differences between the 859xEM EMC Analyzers and the 859xE Spectrum Analyzer families?

The 859xEM EMI Receiver family comes standard with pre-loaded options specifically for EMC pre-compliance measurements. Those options include:

  • Quasi Peak and EMI Average Detectors (Similar to Option 103). 

        Note:  The 103 board that is used in the 9xEM products is a surface mount board with an 85462-xxxxx part number.  This board contains an EMI Average Detector.

  • Narrow Resolution Bandwidths (Option 130)
  • GPIB + Parallel Interface (Option 041)
  • Rom card with limits, correction factors, and setups.
    (08590-10027)