Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

Keysight Instruments Supported with Keysight License Manager

Do not install Keysight License Manager on a Keysight instrument. Keysight License Manager is designed to be installed on an external PC only. Using a LAN connection, the Keysight License Manager can then interact with the instruments below.

The following Keysight instruments are compatible with Keysight License Manager 4.6 M3.

Supported Instruments/Products 

The MXG is a non-Windows based instrument so not all of the functionality of the Keysight License Manager is accessible.

* Infiniium software version 5.00 and above is required to support KLM

Last Updated: Oct 29, 2014