Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

9 Tips for Making Better Resistance Measurements

Digital multimeters include a lot of features to improve the accuracy of resistance measurements. Unfortunately, most of these features add additional measurement time. In order to make good decisions, trading off speed for accuracy, you need to have a good understanding of each type of measurement error and the features incorporated into the multimeter to limit these errors. Following are nine tips for making better resistance measurements.