Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

I/O Libraries Example Programs

These example programs show the basics of how to control Test and Measurement equipment using modern, industry-standard API's.

Once you've got the basics down, accelerate your instrument programming with Command Expert, Keysight's no-charge tool to interactively find and try instrument commands.
 

The following examples are currently available:
 

  • Getting Started - this simple example shows the "basics" of getting connected to and communicating with an instrument
  • Find Devices - shows how to programmatically discover devices that are connected in Connection Expert
  • Error Handling - shows how to handle errors when they occur
  • PXI Information - get details about a PXI device, such as it's chassis and slot number
  • TCP/IP Socket Example - get connected, show details about the connection, and send a command
  • Serial (RS-232) Example - get connected, optionally setting the baud rate, flow control, data size, and parity

 

The following languages and API's are currently provided:

Language Support

Programming
Language

I/O API

C# VISA.NET
VB.NET VISA.NET
C/C++ VISA
MATLAB VISA 
Python PyVISA 

Liens associés

Documents et téléchargements

IO Libraries Suite Example Programs 
I/O examples using C#, VB.NET, C/C++, MATLAB, Python

Programming Example 2016-10-19

null ZIP 840 KB
Old Example Programs 
These old example programs were installed by IO Libraries Suite 16.3 Update 2 and previous releases. They may not work in modern tools, but are provided for reference

Programming Example 2015-05-12

null ZIP 1.42 MB