Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

Can I use VEE to download a trace from my 3562A Dynamic Signal Analyzer?

Yes. There are three formats in which a trace can be downloaded: ASCII format, ANSI floating point binary format and non-standard internal binary format. The ASCII format is the easiest to set up, but is the slowest. The ANSI format is faster and not too difficult to do. The internal binary format is the fastest, but the downloaded data must be interpreted since it is in non-standard format.

Refer to ASCII Example

Refer to ANSI Example

Revision 1.0 16 Dec, 1999 aeh

Liens associés