Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

Is VEE supported on Microsoft Windows 98?

VEE 4.0 (and greater) has been tested and is supported on Windows 98.

VEE uses the Agilent I/O Libraries. The I/O Libraries G.02.02 (and greater) release supports the GPIBinterfaces (82341C, 82341D, 82350A) on Windows 98.

I/O Libraries G.02.02 (and lesser) release does not yet officially support the E8491A Firewire interface on Windows 98.

The latest release of the I/O Libraries is available at http://www.agilent.com/find/iolib

http://www.agilent.com/find/iolib