Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

How do I save my trace data in a comma-separated variable (.csv) file format on an ESA, PSA or EMC spectrum analyzer?

On the front panel of the analyzer, press [File]{Save} and select either the A: (floppy) or C: (internal) drive using the {Dir Up} and {Dir Select} softkeys.

Then use the following softkeys to configure and save the trace data:

  • {Type}{Trace}
  • {Format}{CSV}
  • {Source} either {All Traces}, {Trace 1}, {Trace 2} or {Trace 3}
  • {Name} enter your filename (optional)
  • {Save Now}

If you have saved the file to the floppy drive, you can now transfer the disk to your PC and open the saved file with most spreadsheet programs.