Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

When working with high power setups, is it valid to calibrate at low powers and then increase the power after calibration?

Yes, this is valid as long as the source attenuator setting does not change. It is useful to put the source attenuator into manual mode to ensure it remains the same; however, this does require that the correct value be set to get the desired power range.