Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contate um especialista

8560E/EC Series Spectrum Analyzer Calibration Guide Figure 10-72 Correction

There is an error in the 8560E/EC Calibration Guide for test #59 - "Delayed Sweep Accuracy". Instead of an image of the equipment setup it has an image of the programming diagram for the Mean Power measurement.

Here is the correct image for Figure 10-72 Delayed Sweep Accuracy Test Setup

Correct image for calibration guide Figure 10-72