Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contate um especialista

What's new in Command Expert 1.4 and Update 1

 

 

Command Expert 1.4 Update 1 New Features 
Feature Description
New Features
  • Command Expert can now export C/C++ code targeting IVI-C drivers.
  • You can now add more than 10 sequences to a single Excel workbook. (Note that doing so may impact performance)
  • When adding a new instrument, you can now choose to show only favorite instruments (as defined in Keysight Connection Expert), making it easier to find the instrument you wish to add.
Defects Fixed
  • Drop-down selection lists were not shown for certain IVI-C attributes that have a limited set of valid values. Those lists are now shown.

  

Command Expert 1.4 New Features
Feature Description
Additional Supported Environments
  • Now Supports MATLAB R2014b
  • Now supports LabVIEW 2014
Other Improvements
  • Adds support for IVI-C drivers
  • Improved Excel Add-on that allows the user to have multiple Command Expert sequences per workbook
  • Profiling enhancements
  • Command Expert 1.4 adds support for Multiple Module Instrument addresses used by instruments such as the Keysight M9393A VSA and M9381A VSG.
  • Command Expert has an enhanced instrument discovery service that detects the same instruments detected by Keysight IO Libraries Suite 17.0

 Last Modified: February 7, 2015