Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contate um especialista

What's new in Command Expert 1.2 Update 1?

 

Command Expert 1.2 Update 1 Changes
Feature Description
Additional Supported Enviroments Now Supports MATLAB R2013b, Excel 2013, and LabVIEW 2013 
Defect Fixes
  • Users with the Windows short date format set to "dd-MMM-yy" were not able to download command sets. This has been fixed.
  • LabVIEW 2010 French Version did not update sequence blocks in some cases. This has been fixed.
  • In some cases, Command Expert failed on startup on Czech Windows XP. This has been fixed.
  • Certain text boxes in Command Expert were limited to 512 characters, preventing entry of waveform data in those fields. This limitation has been removed.
  • Running a sequence containing an invalid Excel range caused Excel to stop responding. These sequences now cause an error message and will not run.
  • In some cases, the Excel Add-in would fail to clear a range overlap error message when the overlap was resolved. This has been fixed.
  • In some cases, the Excel Add-in did not behave correctly when On Error was set to Prompt User. This has been fixed.

 Last Modified: September 19, 2013