Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contate um especialista

What are the known issues with Command Expert 1.2?

Known Issues
Issues Workaround/Notes
If Internet Explorer 6 or below is installed, documentation for some commands will not display correctly in Command Expert. Install Internet Explorer 7 or above
When you install Command Expert on a PC with Excel, the Excel Add-on will only be installed for the current user. None; only the current user at the time of the installation will be able to use the Excel Add-on.
While installing Command Expert on 64-bit Windows 7, Windows sometimes displays a dialog box that says "This program may not have installed correctly."

While installing Command Expert on 64-bit Windows 7, Windows sometimes displays a dialog box that says "This program may not have installed correctly." Click the Cancel button in the dialog box that says "This program may not have installed correctly". The Command Expert install will finish without issues.

You can download a Microsoft patch that may correct this issue. See http://support.microsoft.com/kb/978637.

 

Command Expert LabVIEW Add-on: after a reboot of your PC, the first time you drop a Sequence block, there is a long delay before the Command Expert window appears. This delay only happens the first time (after a reboot) that you drop a Sequence block.
Command Expert does not work with the NVIDIA nView Desktop Manager. If the nView Desktop Manager is running when you launch Command Expert, Command Expert will not respond to any mouse clicks. Disable nView when running Command Expert.
When in "streaming mode", the Infiniium 90000A :WAVeform:DATA? command returns streaming data. Command Expert only retrieves the first portion of the streaming data. None
VISA C/C++ code generation for return values that are of the format String Program Data and contain white space is incorrect. The "%#s" format string that is generated will only read until the first white space character, not until the end of the quoted string. Change the format string to "%#t"
If your PC has a supported version of Microsoft Excel installed (Excel 2007 or 2010), and also has Excel 2013 installed, the Command Expert installer will not install the Excel Add-in. Install Command Expert 1.2 Update 1 or later
If the Windows 8 On-Screen Keyboard is enabled and the Command Expert Excel Add-in is installed, then Microsoft Excel may be slow to shut down. Disable the On-Screen Keyboard.

Last Modified: September 27, 2013