Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contate um especialista

N67xx Mainframe Digital Ports

This is an example program that works with the following Model Numbers:

  • N6700B
  • N6701A
  • N6702A
  • N6705A
  • N6705B

The attached files contain an example of how set up the 8 pin digital port on the Keysight N67xx DC Power mainframes. This program allows the user to set the function, the polarity, the fault conditions, read the digital input, and set the digital output.

There are two attached files. One is a compiled exe file that will run on any PC with the Keysight IO Libraries. The second is a Visual Basic 6 program that includes all of the underlying code. This code is free to modify.

Please e-mail any feedback on this example to plsp-power_prod_support@keysight.com

Microsoft is a U.S. registered trademark of Microsoft Corporation.

Documentos e downloads

Compiled Executable File 

Exemplo de programação 2010-06-04

null EXE 16 KB
Source Code 

Exemplo de programação 2010-06-04

null ZIP 12 KB