这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

SystemVue2017 Update 0.1

SystemVue 2017 Update 0.1 addresses the following enhancements and defect fixes. It installs on top of the SystemVue 2017 installation.

RF Design Kit (Spectrasys)

Features Added

  • Added support for LO spur self-mixing where LO spurs mixes with the main LO and appear at the non LO ports of a mixer. See LO Spur LO Mixing for additional information.

Defects Fixed

  • Resolved installer issue to properly install .NET 4.6 when earlier version of .NET 4 exists.
  • Resolved stability issue when using VSA 2018 Beta versions from SystemVue.
  • Fixed crashes associated with noise simulation when using the modulated RF or RF link features.
  • Fixed a frequency comb issue where high carrier count intermod envelops were not created for amplifiers when located after a mixer. This could be seen as incorrect ACPR for stages following a mixer.
  • Fixed issues with the setdisplayunit function. It will now work for power spectral density units dBm/Hz, dBm/MHz, dBW/Hz, and dBW/MHz.

5G Library

Features updated

  • Updated BER measurement part in V5G_DL_Throughput.wsv to support coded BER measurement, rather than payloads BER measurement, according to customers' requirement
  • Updated relevant subnet "V5G_DL_Rcv" to support above feature and also updated affected workspace "V5G_DL_Tx.wsv"

Known issue

Help documentation may not work work after installing Systemvue 2017 Update 0.1.

Workaround: Delete the “SystemVue2017” folder under C:\Users\Account Name\ AppData\Local\Keysight\Help\

* where "Account Name" is your Windows login

SystemVue 2017 Update 0.1 Download

Platform Filename Downloads  Size
Windows (64-bit) SystemVue2017Update0.1.exe Download 167,653,376 bytes (160 MB)

Request a New or Updated License (KSM)

Install Instructions:

Pre-requisite

SystemVue 2017 must be installed and invoked once before you install SystemVue 2017 Updated 0.1.

  1. Download SystemVue 2017 Updated 0.1 installer executable.
  2. Run the installer executable.
  3. Follow the Wizard to complete the installation.

Note: We do not support un-installation of SystemVue 2017 Update 0.1, to un-install you need to completely un-install SystemVue 2017.

Platform Support

Supported Platforms:

  • Windows 7 Enterprise (64-bit)
  • Windows 10 (64-bit)

Licensing

SystemVue requires:

  • Version 2017.01 of the Keysight EEsof EDA licensing software, can be downloaded from here.
  • The licensing server software, lmgrd and agileesofd, to be upgraded to at least the same versions as what are included in the Keysight EEsof EDA Licensing software 2017.01. SystemVue 2017 Update 0.1 will not start if any of these requirements are not met.
    Refer to the License Codeword Version Compatibility Table.

More Information About This Release