这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

航空航天与国防

此内容需要使用支持JavaScript的浏览器和Adobe Flash Player

获得Flash 

集中精力完成重要任务

航空航天与国防行业的任务正在不断发展和变化,但是有一点始终未变,那就是必须要保证那些从事危险工作的人员的人身安全。这项任务能否成功,取决于人员和技术如何适应变化,实现完美融合。随着系统技术日趋复杂,达到这一目标也变得越来越困难。

是德是您成功完成任务的保证。借助是德在测量科学和测试流程中的专业技术,您可以腾出更多时间来处理更重要的问题:执行当前任务并按计划转向未来任务。有是德保证您的系统就绪,您完全可以高枕无忧,从而集中精力完成更重要的任务。

有关是德在航空航天/国防领域的作用的更多信息,请下载免费手册 《是德在航空航天与国防领域的作用》。

查看测量解决方案实例有源天线测试多发射机环境测试信号

1-25 / 52

排序:
Creating Multi-Emitter Scenarios for Radar and Electronic Warfare (EW) Testing - Application Note 
Part 8 of the Radar App Note series focuses on multi-emitter testing of radar and electronic warfare (EW) systems. Realistic testing of these systems depends on the generation of signals that accurately simulate multi-emitter environments consisting of thousands of emitters and millions of pulses per second, all arriving from multiple directions. New technology built into commercial, off-the-shelf signal generators enables developers to generate increasingly complex simulations that get closer to reality and provide deeper confidence in EW system performance.

应用说明 2018-05-31

PDF PDF 1.92 MB
E4438C ESG / E8267D PSG Option 409 GPS Personality - Technical Overview 
An 8-page overview of the E4438C-409 and E8267D-409 Global Positioning System (GPS) personally covering the main features, technical specifications, and ordering information.

技术总览 2017-12-05

Signal Generator Spectral Purity - Application Note 
This application note describes spectral purity and its components. The importance of high spectral purity is explained using industry applications.

应用说明 2017-12-01

PDF PDF 864 KB
是德科技GPS 接收机测试 
是德科技GPS 接收机测试

应用说明 2017-11-29

是德科技PXI 和 AXIe 产品及解决方案 
是德科技PXI 和 AXIe 产品及解决方案

产品目录 2017-11-28

PDF PDF 5.16 MB
是德科技征服千瓦级双象限电源的测试需求 
是德科技征服千瓦级双象限电源的测试需求

应用说明 2017-11-28

是德科技 利用 GPS 信号仿真器进行典型的 GPS 接收机验证测试 
是德科技 利用 GPS 信号仿真器进行典型的 GPS 接收机验证测试

应用说明 2017-11-27

是德科技M8190A任意波形发生器 
是德科技M8190A任意波形发生器

产品资料 2017-11-23

RF Capture and Playback for Improved Communications Jamming - X-COM 
RF Capture and Playback Solutions for Improved Communications Jamming from X-COM and Keysight

Solution Brief 2016-02-11

 
E4360 Modular Solar Array Simulators - Data Sheet 
This data sheet discusses the Keysight E4360 Modular Solar Array Simulator (SAS) which is a dual output programmable dc power source that simulates the output characteristics of a solar array.

产品资料 2015-07-31

Signal Studio for Global Navigation Satellite Systems (GNSS) N7609B - Technical Overview 
Reduce the time you spend on signal simulation with Signal Studio's Keysight-validated and performance-optimized GNSS (GPS, GLONASS, Galileo and Beidou) signals.

技术总览 2014-09-11

Microwave Frequency Up-Converters Extend Signal Simulation to 40 GHz – Synopsis 
Microwave frequency up-converters extend signal simulation to 40 GHz from Synopsis and Keysight

Solution Brief 2014-08-04

 
Using Flexible Digital Modulation Testing for Satellite Regenerative Payloads - Application Note 
This application note focuses on solutions for the issues that create risks in the integration of mixed-signal systems with a mix of software and hardware tools. Examples focus on measurements of error vector magnitude (EVM), which is a key figure of merit for modulated signals implemented in either analog or digital form.

应用说明 2014-08-01

Helping you focus where it counts in aerospace and defense - Brochure 
This brochure covers the latest A/D test resources focused on Radar, EW, Satellite, MicComm and SDR.

手册 2014-08-01

PDF PDF 8.68 MB
Solving the Challenges of Solar Array Simulation - Application Note 
Solving the Challenges of Solar Array Simulation defines the optimal power solution for satellite ground testing.

应用说明 2014-07-31

Improved Methods for Measuring Distortion in Broadband Devices - Application Note 
This paper illustrates that, in broadband commercial and defense systems, it is more important than ever to characterize them for non-linearity. It is also important to understand the mechanisms that create these non-linearities and the characteristics of the waveforms that cause them. We focus on the primary tests used to determine the level of a system’s distortion products and how they result in Intermodulation Distortion (IMD) and Intermodulation Distortion Noise (IMDN). Looking at the method to evaluate the effect of IMD in a communication system under real data traffic conditions, Noise Power Ratio (NPR), we see measures of the IMD as a function of data traffic conditions in a wideband or multi-channel communications channel.

应用说明 2014-07-31

PDF PDF 2.17 MB
RF Interference Troubleshooting with RF Editor and Playback Solution - X-COM 
RF Interference Troubleshooting with RF Editor and Playback Solution from X-COM and Keysight

Solution Brief 2014-05-14

 
RF Test Solutions – WinSoft 
Military and Commercial RF Test Solutions from WinSoft and Keysight.

Solution Brief 2014-05-14

 
In-Orbit Satellite Testing – SED Systems 
In-Orbit Satellite Testing Solutions from SED Systems and Keysight Technologies

Solution Brief 2014-05-07

 
COTS-Based Functional ATE – G Systems - Solution Brief 
Commercial-off-the-Shelf (COTS) based Automated Functional Test Solutions from G Systems and Keysight.

Solution Brief 2014-04-29

 
Satellite Test Solution – AAI 
Satellite Payload and Panel Test Solution from AAI and Keysight Technologies

Solution Brief 2014-04-09

 
Realistic Ultra Wideband Radar Signal - Demo 
Testing of radar systems can be extremely time-consuming and expensive. Radar transceivers must be designed and tested with realistic environment and jamming scenarios, which often involve costly outdoor ranges, chambers, and real-time hardware simulators.

基本演示 2013-11-25

 
A new approach for multi-emitter test signal generation – Article 
A new capture and playback approach generates multi-emitter test signals using a combination of COTS test equipment and simulation software.

文章 2013-11-15

 
Radar, EW & ELINT Testing: Identifying Common Test Challenges - Application Note 
This application note reviews some of the latest test equipment for radar, EW & ELINT systems. Since this is a complex subject, we begin with a brief review of the fundamental radar and EW/ELINT challenges.

应用说明 2013-04-29

是德航天/国防雷达测试解决方案 
This brochure describes Keysight’s commitment to, and solutions for, the Aerospace/Defense market worldwide.

手册 2011-06-24

PDF PDF 1.84 MB

1 2 3 下一页