这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

是德科技蜂窝测试技术

是德科技公司是全球领先的测试与测量公司,可以提供全方位的设计、测试和管理解决方案。这些解决方案覆盖整个蜂窝技术领域――从传统1G系统到3G系统(例如HSPA),再到3GPP 长期演进技术(LTE)和1xEV-DO。是德的产品适用于从早期设计与开发、批量制造到网络部署和服务保障的全过程。推动蜂窝技术的创新与发展,是德为您披荆斩棘!

 

#5G #LTE-Advanced (LTE-A) #LTE测试 #毫微微蜂窝基站测试 #包络跟踪功率放大器 #HSPA和HSPA+ #W-CDMA #TD-SCDMA #GSM、GPRS、EGPRS和EDGE/Evo #1xEV-DO #cdma2000®/CDMA #多标准无线(MSR)#全球导航卫星系统(GNSS)和辅助 GNSS(A-GNSS)设计与测试解决方案 #TDMA

查看相关视频(优酷) 

151-175 / 356

排序:
Agilent Technologies announces 160-MHz bandwidth and real-time capability for MXA signal analyzer 
Agilent Technologies announced significant enhancements to its midrange N9020A MXA X-Series signal analyzer. New options for 160-MHz analysis bandwidth and real-time spectrum analyzer (RTSA) capability address the challenges of measuring interference in the next generation of heterogeneous wireless networks.

新闻资料 2013-06-04

 
Agilent Technologies Unveils System Design Tools for Satellite Communications and Navigation 
Agilent announces two reference libraries for SystemVue, its premier platform for communications and aerospace/defense systems design.

新闻资料 2013-06-03

 
N7609B Signal Studio for GNSS 
Keysight YouTube videos for GNSS

基本演示 2013-05-21

 
Agilent Technologies Unveils Beidou GNSS Signal Simulation at International Wireless Symposium 
Agilent Technologies announced that it has enhanced the capabilities of its Signal Studio for Global Navigation Satellite Systems (GNSS) software and added real-time multi-satellite simulation of China's Beidou system.

新闻资料 2013-04-15

 
Agilent PXT Wireless Communications Test Set Selected by Tri-L Solutions for LTE Over-the-Air Test 
Agilent Technologies Inc. (NYSE: A) today announced that Tri-L Solutions Inc. has selected Agilent's PXT wireless communications test set and integrated it with Tri-L Solutions SmarTest measurement software for testing LTE over the air.

新闻资料 2013-04-08

 
阅读 42 位 LTE 专家共同倾力撰写的 LTE 著作,了解 LTE 的历史背景与最新发展及相关测量 
是德科技发布关于长期演进(LTE)的最新著作,对 3GPP LTE 蜂窝新技术进行了深入分析,并提供了各种设计和测试技巧,以及必要的设备。

促销资料 2013-01-24

 
阅读 42 位 LTE 专家倾力撰写的 LTE 著作,了解 LTE 的历史背景与最新发展及相关测量 
是德科技关于长期演进(LTE)的新书深入探讨了 3GPP LTE 蜂窝方面的新技术,并介绍了设计、测试技巧以及所需的设备。

促销资料 2013-01-24

 
Agilent Technologies Introduces Industry's First LTE-Advanced 8x8 MIMO Signal-Generation and Analysi 
Agilent Technologies Introduces Industry's First LTE-Advanced 8x8 MIMO Signal-Generation and Analysis Solutions

新闻资料 2013-01-03

 
Frequency Agile Complex Signal Simulation with the Keysight M8190A Arbitrary Waveform Generator 
The Keysight M8190A Arbitrary Waveform Generator (AWG) generates complex, realistic test signals needed for today's sophisticated signal simulation and system test. Keywords: Arbitrary Waveform Generator,Long play time, frequency agile switching,signal scenario generator

应用说明 2012-11-29

PDF PDF 636 KB
89601B/BN-BHD LTE FDD and -BHE LTE TDD调制分析和89600B VSA技术概述 
This technical overview describes LTE FDD and LTE TDD modulation analysis using Option BHD or BHE.

技术总览 2012-11-22

Agilent Technologies and CATR (TMC) to Collaborate on TD-LTE MIMO  
Agilent Technologies Inc. (NYSE: A) announced a memorandum of understanding has been signed with the China Academy of Telecommunication Research (Telecommunication Metrology Center), or CATR (TMC). The two organizations have agreed to work together on TD-LTE MIMO over-the-air (OTA) test research.

新闻资料 2012-09-13

 
Agilent Technologies Announces Wireless Communications Test Set with Innovative Multiport Adapter 
Agilent Technologies introduced the E6607B EXT wireless communications test set and companion E6617A multiport adapter. Optimized for non-signaling testing, the EXT/MPA combination increases test throughput and reduces the cost of test in the manufacturing of current- and next-generation smartphones and tablets that contain multiformat and multiband technologies.

新闻资料 2012-08-01

 
EXT Wireless Communications Test Set Non-signaling Test Overview 
This application note explains how non-signaling test methods make it possible for manufacturers to reduce both test times and test equipment costs across a range of wireless technologies

应用说明 2012-08-01

PDF PDF 290 KB
Agilent Technologies Accelerates Early Wireless Design Verification with New Release of SystemVue 
Agilent will demonstrate SystemVue 2012.06 along with a range of solutions for everything from circuit-level modeling through system verification for general RF, microwave, 4G communications, and aerospace/defense applications at DAC2012 (Booth 313), June 3-7, in San Francisco. SystemVue 2012.06 will also be demonstrated at IMS 2012/IEEE MTT-S (Booth 1015), June 19-21, in Montr al, Canada. A range of premier partner solutions will be available on Agilent Avenue and throughout the event area.

新闻资料 2012-06-05

 
免费下载最新的“强大的 X 系列”应用指南 
免费下载最新的“强大的 X 系列”应用指南

促销资料 2012-05-21

 
Agilent Technologies Announces Voice-over-LTE Test System Developed with Brüel & Kjær 
Transporting voice over a packet-based LTE cellular infrastructure poses challenges that make voice-quality testing essential. The Agilent and Brüel & Kjær solution combines standards-based test methods with real-world base station emulation, RF test and functional test to ensure that VoLTE phones will meet user's expectations.

新闻资料 2012-05-10

 
MIMO Over-The-Air Research, Development, and Testing 
International Journal of Antennas and Propagation, May 2012 article provides information on the many challenges of identifying the optimal channel models and test method(s), for MIMO

文章 2012-05-09

 
Spectrum and Signal Analyzer Measurements and Noise Application Note 1303 
Noise is the classical limitation of electronics. In this application note, the characteristics of noise and its direct measurement are discussed in detail.

应用说明 2012-05-04

PDF PDF 2.06 MB
Agilent Technologies Enhances FieldFox RF Analyzers with Options for Measuring Time Domains and Chan 
Agilent will demonstrate its new FieldFox options, along with solutions that cover everything from circuit-level modeling through system verification for general RF, microwave, 4G communications, and aerospace/defense applications at IMS 2012/IEEE MTT-S (Booth 1015), June 19-21, in Montr�al, Canada. A range of premier partner solutions will also be available on Agilent Avenue and throughout the event area.

新闻资料 2012-05-01

 
Agilent Technologies Introduces 6-GHz Signal Generators with Industry-Best Performance 
Today's aerospace/defense environment requires enhanced radar performance to detect weak signals at long distances. To provide the pure and precise signals needed to test these designs, the MXG uses an innovative triple-loop synthesizer to deliver phase noise performance of -146 dBc/Hz at 1 GHz and 20 kHz offset. For developers of radar components such as mixers and analog-to-digital converters, the MXG also features industry-leading spurious performance of -96 dBc at 1 GHz.

新闻资料 2012-05-01

 
Agilent Technologies Named Oscilloscope Company of the Year 
The award is based on Frost & Sullivan's recent analysis of the oscilloscope market. Frost & Sullivan ranked Agilent as the No. 2 company in 2009, but its rapid revenue growth since then has made it the leader in market penetration.

新闻资料 2012-04-25

 
免费下载最新的“强大的 X 系列”应用指南 
Learn about the Power of X – Keysight’s suite of test products that help you get your innovative, higher-performing designs to market before your competition.

促销资料 2012-03-29

 
Two-Stage Over-the-Air (OTA) Test Method for LTE MIMO Device Performance Evaluation 
International Journal of Antennas and Propagation, February, 2012, article introduces a novel, flexible, and cost-effective method for measuring MIMO OTA using a two-stage approach.

文章 2012-03-28

 
Agilent Technologies Introduces Wireless Link for Remote Monitoring and Data Logging with Handheld 
Agilent Technologies Inc. announced the introduction of a wireless connectivity solution that links up to three Agilent handheld digital multimeters to smartphones, tablets and PCs.

新闻资料 2012-03-01

 
Agilent Technologies Announces Test Software for Equipment Based on Altair TDD/FDD LTE Chipset 

新闻资料 2012-02-28

 

以前 1 2 3 4 5 6 7 8 9 10 ... 下一页