検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

携帯電話

原因究明。 それがすぐに可能です。 特別な現象が得られたことがすぐにわかります。 キーサイト・テクノロジーの礎は、優れたハードウェア、ソフトウェア、人材の融合です。 測定技術分野のリーダーとして75年以上の実績があるキーサイトが作成した測定器とデザインソフトウェアにお任せください。

新しい携帯電話テクノロジーと既存の携帯電話テクノロジーの両方に渡る革新が続くことで、モバイルネットワーク/デバイスのデザイン/テストにさまざまな問題が生じます。 キーサイト・テクノロジーは、世界有数の電子計測器メーカーとして、シミュレーション、研究開発、デザイン検証、プリコンフォーマンス、コンフォーマンス、製造から、ネットワークの配備およびサービス保証までのライフサイクル全体に渡る携帯電話のテスト/デザインソリューションを豊富に取り揃え、最先端を走り続けています。

キーサイトは、デザインに何を取り入れれば最新の携帯電話規格に準拠できるのかを知っています。 キーサイトは、3GPPなどの有力な無線規格団体や最先端の5Gフォーラム/コンソーシアムのメンバーとして活動しているので、従来の1Gから最新の4Gテクノロジーまでの規格に準拠した最先端の携帯電話のテスト/デザインツールを提供できます。また、シミュレーションやテストに関する5Gの研究に対応するデザイン/テストソリューションを豊富に取り揃え、常に業界をリードしています。

測定器は将来も使用できるようにデザインされているので、テクノロジーの変化に応じて容易に進化して、最先端の課題に対応できます。 今日の研究開発から製造および将来の配備まで一貫した測定技術が提供されるので、お客様の投資を有効に活用できます。

キーサイトのデザイン/テストのエンジニア/専門家は、お客様のチームに対するアドバイス、支援、強化を世界中で行うことができます。 5G携帯電話MIMO無線LANテストに関するキーサイトの専門知識は、技術記事、アプリケーションノート、ウェブキャストで今すぐご覧いただけます。

YouTubeビデオを見る 

1-25 / 30

並べ替え
The Problems of Testing 5G, Part 1 - Article Reprint by Moray Rumney 
This article introduces the challenges of testing 5G devices, with a discussion of New Radio (NR)

記事 2018-01-29

PDF PDF 827 KB
Paving The Way For 5G Realization and mmWave Communication Systems – Article Reprint 
This article Paving The Way For 5G Realization and mmWave Communication Systems first appeared in the April 2016 edition of Microwave Journal. Reprinted with kind permission from Microwave Journal.

記事 2016-05-03

PDF PDF 2.90 MB
Flexible Testbed for 5G Waveform Generation and Analysis 
While LTE and LTE-Advanced are still being deployed, research into next generation wireless networks is already in high gear.

記事 2015-11-13

 
5G air interfaces need channel measurements 
EDN, Oct 31, 2015 article by Sheri DeTomasi discusses characterizing the radio channel to understand how the new 5G signals will propagate and describes a system that will provide the needed insights.

記事 2015-10-31

 
5G set to dramatically impact test and measurement 
Canadian electronics, Oct 19, 2015 article by Roger Nichols discusses the challenges of testing in the investigations of the different 5G technologies.

記事 2015-10-19

 
Modular Tester Performs 5G Channel Sounding 
The 5G Channel Sounding Reference Solution test system features compact instrument modules and multiple software packages to generate and analyze complex waveforms for characterizing 5G wireless communications channels.

記事 2015-08-04

 
The key to early 5G investigation – test tools for new network paradigms 
Electronic Products and Technology, May 2015 article discusses the needs of 5G, areas of investigations and available test tools to make it happen

記事 2015-05-19

 
mmWave MIMO Channel Sounding for 5G: Technical Challenges and Prototype System 
In this paper, ww focus on how to setup mmWave MIMO channel sounding system with commercial instruments to fulfill the major technical challenges.

記事 2014-12-18

 
MIMO Over-The-Air Research, Development, and Testing 
International Journal of Antennas and Propagation, May 2012 article provides information on the many challenges of identifying the optimal channel models and test method(s), for MIMO

記事 2012-05-09

 
Two-Stage Over-the-Air (OTA) Test Method for LTE MIMO Device Performance Evaluation 
International Journal of Antennas and Propagation, February, 2012, article introduces a novel, flexible, and cost-effective method for measuring MIMO OTA using a two-stage approach.

記事 2012-03-28

 
Defining the 4G PHY Architecture Design Challenges 
EE Times design article (Part 1) on defining the 4G PHY architecture design challenges.

雑誌記事 2011-12-05

 
Using SystemVue to Overcome 4G Challenges 
EE Times design article (Part 2) on using SystemVue to overcome 4G challenges.

雑誌記事 2011-12-04

 
LTE-Advanced…Already? 
Article reprint from OSP magazine detailing the additional changes LTE-Advanced brings to the Network already working to implement 3GPP LTE.

記事 2011-09-01

PDF PDF 695 KB
Don't worry, be happy: Design, test, verification support for LTE-Advanced is here 
Link to Agilent product review in the February 2011 EETimes.

記事 2011-02-14

 
The MIMO Antenna: Unseen, Unloved, Untested! 
Microwave Journal (August 2010) article (.pdf) written by Agilent’s Moray Rumney. With the shift of MIMO from theory to real world this article focuses on performance testing in real world conditions.

記事 2010-08-20

PDF PDF 693 KB
Measuring MIMO In LTE Tx And Rx Tests 
Find the right combination of LTE test instruments and techniques to evaluate the performance of Long Term Evolution (LTE) components and systems under real-world conditions. A link to the MWJ article by Agilent.

記事 2010-08-18

 
A primer on MIMO in LTE 
An article in Electronic Products, written by Agilent’s Jan Whitacre, exploring the special employment of multiple-input, multiple-output radios to utilize spectrum in Long Term Evolution (LTE) systems.

記事 2010-02-01

 
Using a design-to-test capability for LTE MIMO  
Article written for RF DesignLine by Keysight experts explains how system-level simulation helps engineers gain valuable insight into design sensitivities of LTE MIMO systems.

事例紹介 2009-07-10

 
IMT-Advanced:第4 世代の無線通信が具体化 
いわゆる3.5G、3.75G、3.9G 規格の開発に加 えて、第4 世代(4G)に対する期待が高まっています。また、3GPPのワーキング・グループの会合に続いて、4G 無線通信に関するワークショップが、中国のシンセンで開催されました。

記事 2009-05-18

PDF PDF 961 KB
TD-LTE Technology And Its Measurements 

特集記事 2009-05-14

PDF PDF 447 KB
GPS: making a play for femtocells 
This article from Microwave Engineering Europe Jan/Feb 2009 discusses the issues that arise when integrating GPS into femtocells and outlines the test and verification requirements that this introduces.

記事 2009-04-16

 
MIMO and the Battle Between LTE and WiMAX™ 
Link to April 10, 2009 Microwave Journal executive interview with Andy Botka and Carla Feldman regarding the PXB MIMO Receiver Test and the broader issue of LTE and WiMAX development.

記事 2009-04-10

 
Test solutions soup up for 4G 
Link to April 9, 2009 Microwave Journal editorial. Test equipment manufacturers are providing more capability by relying on the latest hardware and software for feature-rich and easy to use solutions with impressive raw performance.

記事 2009-04-09

 
Expert Advice: The Importance of Average vs. Peak Performance in Cellular Wireless 
The average efficiency of the cell remains much lower than the peaks. November 2008 article by Moray Rumney linked with permission by Microwave Journal.

記事 2008-11-17

 
Agilent Measurement Journal, Issue 6, September 2008 
Using a few words to convey a deeply-held spirit - read more about Agilent's contributions to the Olympic Games in Beijing in communications, electronics, life sciences, and chemical analysis.

雑誌記事 2008-09-01

PDF PDF 4.29 MB

1 2 次へ