이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

무선 단말 통신

Keysight Technologies, the world’s premier measurement company, offers a full range of design, test, and management solutions that span the range of cellular technologies—from legacy 1G systems through 3G systems such as HSPA to 3GPP Long Term Evolution (LTE) and 1xEV-DO. Keysight products cover the lifecycle from early design and development, through volume manufacturing, to network deployment and service assurance. So as you take cellular forward, Keysight clears the way.

유튜브 동영상 보기 

상세 분류

상세분류 제거

산업/기술

분야별 검색결과

제품 카테고리별

1-25 / 165

정렬방식:
5G Waveform Evaluations For mmWave Communication Using SystemVue 
This application note evaluates and compares the performance of various state-of-the art waveforms in the presence of hardware impairments.

어플리케이션 노트 2017-11-04

PDF PDF 1.15 MB
Massive MIMO: Answering Some Common Questions - White Paper 
The promise of new digital technologies to take full advantage of a rich radio channel continues to drive innovation in the industry with regards to 5G and massive MIMO.

어플리케이션 노트 2017-07-13

5G Massive MIMO로의 발전: 빔포밍 시뮬레이션 및 측정 - 애플리케이션 개요(영어) 
매우 복잡한 시스템을 시뮬레이션, 설계 및 테스트하는 데 필요한 도구를 포함하여 5G 에코시스템 내에서 Massive MIMO 기술을 개발 및 구현하기 위한 새로운 요구사항을 개략적으로 소개합니다.

어플리케이션 노트 2017-02-23

Evolution of the Radio Access Network: Fronthaul Test and Monitoring - Application Brief 
Overview of fronthaul test and monitoring solutions from Keysight Technologies for Radio Access Networks (RAN).

어플리케이션 노트 2017-02-23

PDF PDF 386 KB
Optimize your wideband test solution 
download new application note: Optimize your wideband test solution

어플리케이션 노트 2017-02-21

 
FPGA Implementation of a LUT-Based Digital Pre-Distortion - Application Note 
This application note demonstrates the implementation of a signal transformation using a lookup table (LUT). This program transforms a sawtooth signal into a sinusoidal.

어플리케이션 노트 2017-01-05

MIPI® RFFE 및 SPI 버스 테스트 기법으로 PA/FEM 콤포넌트 테스트 효율성 증가 (영어) 
S8900A PA 테스트 솔루션은 무선 모바일 디바이스용 RF 전력 앰프/프런트 엔드 모듈(PA/FEM)을 테스트하기 위한 차세대 소프트웨어를 소개합니다.

어플리케이션 노트 2016-12-16

Testing 5G: Time to Throw Away the Cables - Article Reprint Microwave Journal 
This article describes the test challenges of 5G technology, and sets the scene for what lies ahead to test 5G at mmWave frequencies, almost all over the air (OTA) without cables.

어플리케이션 노트 2016-11-30

PDF PDF 3.25 MB
Bluetooth Audio Measurement with the U8903B Performance Audio Analyzer - Application Note 
This article focuses on the Bluetooth audio measurement applications of the U8903B performance audio analyzer. Bluetooth audio is also part of the whole audio measurement and analysis ecosystem.

어플리케이션 노트 2016-01-28

Increase Power Amplifier Test Throughput with the Keysight PXIe Vector Signal Analyzer and Generator  
This application note overview provides an overview of the challenges and recommended solutions to increase the speed of power amplifier test.

어플리케이션 노트 2015-09-27

Testing Voice Over LTE (VoLTE) Phones - Application Note 
This application note explains a solution for testing voice over LTE (VoLTE) phones that is well-suited for LTE mobile phone developers, test engineers, and test lab personnel.

어플리케이션 노트 2015-09-14

PDF PDF 4.46 MB
Correlating Microwave Measurements between Handheld and Benchtop Analyzers - Application Note 
This application note discusses the powerful capabilities of modern-day handheld analyzers and includes measurement comparisons between FieldFox handheld analyzers and several benchtop instruments.

어플리케이션 노트 2015-08-27

Precision Validation, Maintenance and Repair of Satellite Earth Stations FieldFox Handheld Analyzers 
This application note describes breakthrough technologies that have transformed the way systems can be tested in the field while providing higher performance, improved accuracy and capability.

어플리케이션 노트 2015-08-24

Latest 5G Application Notes, White Papers, Tutorials, and more 
Keysight wireless design and test tools enable the exploration of new technologies needed for next-generation 5G communications.

어플리케이션 노트 2015-08-18

 
W-CDMA Dynamic Power Analysis Using the 8960 - Application Note 
This document illustrates how to use the dynamic power analysis measurement in the Keysight 8960 test set to measure user equipment (UE) power sequences.

어플리케이션 노트 2015-07-31

PDF PDF 379 KB
Techniques for Precise Measurement Calibrations in the Field - Application Note 
This application note discusses recent advances in VNA calibration and compares measurements made on a FieldFox analyzer using different calibration types for a variety of RF and microwave devices.

어플리케이션 노트 2015-05-22

Techniques for Precise Power Measurements in the Field - Application Note 
This application note will discuss techniques for measuring average and peak power and the associated equipment options available for field testing.

어플리케이션 노트 2015-05-22

현장의 정밀 케이블 및 안테나 측정을 위한 기법 - 어플리케이션 노트 (영어) 
이 어플리케이션 노트는 FieldFox 핸드형 분석기를 사용한 케이블 및 안테나 테스트를 위한 측정 및 교정 기법을 소개합니다.

어플리케이션 노트 2015-05-15

Techniques for Precise Interference Measurements in the Field - Application Note 
This app note discusses the different types of interference in current and new systems and methods to measure a variety of interference types using spectrum analyzers such the FieldFox Series.

어플리케이션 노트 2015-03-30

RF 전력 앰프 테스트를 위한 솔루션 어플리케이션 노트 

어플리케이션 노트 2015-01-27

 
전력 앰프의 Envelope Tracking 구현을 위한 솔루션 어플리케이션 노트 

어플리케이션 노트 2015-01-27

 
Speed Time to Market with Consistent Measurements from R&D Through Manufacturing - Application Note 
This white paper describes the benefits of having a choice of bench top or modular instruments that are supported by common software applications.

어플리케이션 노트 2014-11-17

Achieving Accurate E-band Power Measurement with Keysight E8486A Waveguide Power Sensors 
E-band spectrum application has been gaining more application interests in the recent years. E8486A addresses the requirement for accurate RF power measurement in the mm-wave applications.

어플리케이션 노트 2014-08-04

Solutions for LTE-Advanced Manufacturing Test - Application Note 
This “Solutions for LTE-Advanced Manufacturing Test” application note gives insight into how to better understand the requirements for LTE-Advanced Carrier Aggregation manufacturing test.

어플리케이션 노트 2014-08-04

GNSS Technologies and Receiver Testing - Application Note 
This application note provides information on GNSS technologies including GPS, Compass, Beidou, Galileo, and Glonass, along with the related receiver test challenges and solutions.

어플리케이션 노트 2014-08-03

1 2 3 4 5 6 7 다음