Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contate um especialista

Wireless Connectivity

Our engineers, experts in test, develop equipment and systems ahead of the technology wave— clearing the path for you to develop the components, modules and devices that make our connected world possible. Keysight participates in many of the standards organizations and works with countless design, development, integration and manufacturing engineers to provide the best tools in the industry. Greater insight. Greater confidence. Accelerate next-generation wireless.

A full portfolio of test and design solutions from Keysight also spans the range of cellular technologies; LTE, 4G LTE, MIMO, HSPA, HSPA+, and more.

Explore os vídeos do YouTube 

Refine the List

Mercado/Tecnologia

By Type of Content

Categoria de Produto

151-175 de 411

Sort:
Agilent Technologies' Bluetooth® Low-Energy RF Test Solution Speeds Development of Devices Based on  
Bluetooth low-energy technology enables long operational life with minimal power consumption for applications such as mobile communications, sports and fitness, health care, security and home entertainment.

Materiais para imprensa 2012-05-29

 
N5182A and N5162A MXG ATE Vector Signal Generators - Data Sheet  
Complete N5182A and N5162A MXG ATE performance specifications are available in the data sheet.

Folha de Dados 2012-05-21

MIMO Over-The-Air Research, Development, and Testing 
International Journal of Antennas and Propagation, May 2012 article provides information on the many challenges of identifying the optimal channel models and test method(s), for MIMO

Artigo 2012-05-09

 
Agilent Introduces 6-GHz Signal Generators with Industry-Best Performance 

Materiais para imprensa 2012-05-01

 
Agilent Technologies Introduces 6-GHz Signal Generators with Industry-Best Performance 
Today's aerospace/defense environment requires enhanced radar performance to detect weak signals at long distances. To provide the pure and precise signals needed to test these designs, the MXG uses an innovative triple-loop synthesizer to deliver phase noise performance of -146 dBc/Hz at 1 GHz and 20 kHz offset. For developers of radar components such as mixers and analog-to-digital converters, the MXG also features industry-leading spurious performance of -96 dBc at 1 GHz.

Materiais para imprensa 2012-05-01

 
Agilent Technologies Named Oscilloscope Company of the Year 
The award is based on Frost & Sullivan's recent analysis of the oscilloscope market. Frost & Sullivan ranked Agilent as the No. 2 company in 2009, but its rapid revenue growth since then has made it the leader in market penetration.

Materiais para imprensa 2012-04-25

 
N4010A Wireless Connectivity Test Set - Brochure 
The N4010A is the first test solution to deliver the ability to test Bluetooth, Bluetooth EDR, Bluetooth low energy, WLAN, and ZigBee in a single, easy-to-use, desk-top box.

Brochura 2012-03-30

PDF PDF 6.76 MB
Two-Stage Over-the-Air (OTA) Test Method for LTE MIMO Device Performance Evaluation 
International Journal of Antennas and Propagation, February, 2012, article introduces a novel, flexible, and cost-effective method for measuring MIMO OTA using a two-stage approach.

Artigo 2012-03-28

 
Tackling MIMO Design and Test Challenges for 802.11ac WLAN 
This article from Microwave Journal shows how the system engineer can use system simulation to help understand the design performance and design requirements needed to achieve transmitter system-level metrics such as EVM.

Artigo 2012-03-11

 
Using a Network and Impedance Analyzer to Evaluate 13.56 MHz RFID Tags and Readers/Writers 
For engineers who work in RFID antenna design and test, this note discusses testing RFID antenna characteristics such as impedance and resonant-frequency with network and impedance analyzers.

Nota de aplicação 2012-02-08

Testing broadband CATV amplifiers with true wideband channel rasters 
The most efficient way to measure amplifier EVM or MER is to apply a complex wideband signal generated by the M8190A and measure the resulting output with a signal analyze.

Nota de aplicação 2012-01-31

PDF PDF 456 KB
Evaluating Fluorescent Lighting Interference on Passive UHF RFID Systems - Application Note 
This paper highlights how the use of N934xC handheld spectrum analyzers are an effective way to determine if the effects of fluorescent lighting is impacting an RFID system

Nota de aplicação 2011-11-30

Agilent Technologies Introduces Signal Processing Libraries for 802.11ac WLAN and 60-GHz 802.11ad  
Agilent Technologies Inc. (NYSE: A) today released SystemVue 2011.10, the latest update to the leading design environment for wireless physical-layer architects.

Materiais para imprensa 2011-11-16

 
Agilent Technologies Introduces Innovative Multi-Measurement Signal Analyzer Capability for Wireless 
Agilent Technologies Inc. (NYSE:A) today announced that an innovative, new multi-measurement capability is being added to its 89600 VSA software, enabling simultaneous signal analysis of multiple carriers and signal formats for more efficient testing and deeper signal insight in wireless test.

Materiais para imprensa 2011-11-15

 
802.11ac Wireless LAN: what’s new and the impact on design and test 
EE times article by Agilent’s Mirin Lew describing the 802.11ac, the technical challenges and comparisons to earlier technologies.

Artigo 2011-11-09

 
Agilent Technologies' PXA Signal Analyzer Now Enables Wideband Measurement with up to 900  
Agilent Technologies Inc. (NYSE:A) today announced that its high-performance PXA signal analyzer now supports up to 900 MHz of intermediate-frequency bandwidth, enabling it to act as a broadband down converter for analysis of wideband communications and radar signals in aerospace and defense applications.

Materiais para imprensa 2011-09-20

 
Agilent Technologies Introduces Wideband DPD Modeling Platform for LTE-Advanced, 802.11ac  
Agilent Technologies Inc. (NYSE: A) today announced the newest release of its W1716 Digital Pre-Distortion Builder (DPD) software, designed to enable the high levels of wireless performance necessary for emerging wideband standards such as LTE-Advanced and IEEE 802.11ac.

Materiais para imprensa 2011-08-31

 
Digital Audio Broadcasting Receiver Testing Solutions - Demo Guide 
This document discusses the measurement configurations and procedures for DAB receiver RF performance test using Keysight instruments, according to BS EN 50248.

Demonstração 2011-07-27

PDF PDF 2.90 MB
89601B/BN-B7Y 802.16e OFDMA & B7S 802.16-2004 OFDM, 89600 VSA Software - Technical Overview 
This technical overview provides RF and baseband engineers the industry's most comprehensive OFDMA and OFDM PHY layer analysis tools for the IEEE-802.16 standard with Option B7Y or B7S.

Visão Técnica 2011-06-11

PDF PDF 1.19 MB
MIMO Tx/Rx Test Solutions - Selection Guide 
For RF engineers working with MIMO implementations in LTE. Determine the right set of Keysight products to help validate MIMO coding and the quality of MIMO signal transmission.

Guia de seleção 2011-05-31

Frost & Sullivan recognizes Agilent 
with the 2011 Award for Market Share Leadership for emerging as the leader in the global wireless test equipment market through a range of products, market-focused approach and customer-oriented solutions.

Materiais para imprensa 2011-05-26

 
Agilent Technologies Acknowledged for Leadership in Wireless Test Market  
Agilent Technologies Inc. (NYSE: A) has received this year's Frost & Sullivan award for market-share leadership in global wireless test equipment.

Materiais para imprensa 2011-05-25

 
N6155A & W6155A ISDB-T with Tmm Measurement Application, Self-Guided Demonstration 
This guide demonstrates the measurement and modulation analysis capabilities of the N/W6155A ISDB-T application and its use in evaluating and manufacturing digital video devices.

Demonstração 2011-05-03

PDF PDF 2.38 MB
Infiniium Oscilloscopes Performance Guide  
Infiniium Link to 89601A Software, Performance Guide.

Nota de aplicação 2011-03-31

Agilent Extends Wireless Leadership with First-To-Market Support for 802.11ac Design and Analysis 
Agilent Technologies announces that its 89600B vector signal analysis software is now able to test 802.11ac signals. This is the first dedicated 802.11ac signal analysis solution on the market.

Materiais para imprensa 2011-03-17

 

Voltar 1 2 3 4 5 6 7 8 9 10 ... Avançar