Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Wireless Connectivity

Insight. It comes upon you in a flash. And you know at once you have something special. At Keysight Technologies, the foundation is our unique mix of hardware, software and people. You can count on test equipment and design software that is built on more than 75 years of leadership in measurement science. The continuing innovation across new and existing wireless technologies presents challenges in designing and testing of components, modules and devices that make our connected world possible. As the world’s leading electronic measurement company, Keysight continues to be at the forefront offering a full portfolio of test and design solutions that span the entire lifecycle – from simulation to R&D, design verification and pre-conformance, conformance, manufacturing, through network deployment and service assurance.

We know what it takes for your designs to meet the latest standards. As an active member of the wireless standards bodies that define the technologies, we have been at the forefront of providing standard-compliant wireless test and design tools across all the technologies from Bluetooth to 60 GHz 802.11ad. We design our instruments to be future-proof, making it easier for you to evolve with changing technologies and stay on the leading edge. You can carry your investment forward with consistent measurement science that spans research and development today and extends to manufacturing and deployment in the future. Our engineers, experts in design and test, are available to advise, assist and augment your teams all around the world. Our expertise is also readily available through white papers, application notes and webcasts for IoT, 5G, Cellular, MIMO and WLAN Test.

Keysight RF and Digital Learning Center - A commitment to learning with industry experts

Explore YouTube Videos 

Refine the List

By Industry/Technology

By Type of Content

By Product Category

151-175 of 412

Sort:
Agilent Technologies Announces Wireless Communications Test Set with Innovative Multiport Adapter 
Agilent Technologies introduced the E6607B EXT wireless communications test set and companion E6617A multiport adapter. Optimized for non-signaling testing, the EXT/MPA combination increases test throughput and reduces the cost of test in the manufacturing of current- and next-generation smartphones and tablets that contain multiformat and multiband technologies.

Press Materials 2012-08-01

 
EXT Wireless Communications Test Set Non-signaling Test Overview 
This application note explains how non-signaling test methods make it possible for manufacturers to reduce both test times and test equipment costs across a range of wireless technologies

Application Note 2012-08-01

PDF PDF 290 KB
Agilent Technologies Accelerates Early Wireless Design Verification with New Release of SystemVue 
Agilent will demonstrate SystemVue 2012.06 along with a range of solutions for everything from circuit-level modeling through system verification for general RF, microwave, 4G communications, and aerospace/defense applications at DAC2012 (Booth 313), June 3-7, in San Francisco. SystemVue 2012.06 will also be demonstrated at IMS 2012/IEEE MTT-S (Booth 1015), June 19-21, in Montr al, Canada. A range of premier partner solutions will be available on Agilent Avenue and throughout the event area.

Press Materials 2012-06-05

 
WiMAX Receiver Basics: Operation of a Dual Channel WiMAX Receiver 
The diagram shows a simplified version of a typical WiMAX™ mobile station (MS) receiver. The bold dashed lines indicate the major feedback loops. As we work through the design, we can identify how these impact testing.

Application Note 2012-06-05

 
Agilent Technologies' Bluetooth® Low-Energy RF Test Solution Speeds Development of Devices Based on  
Bluetooth low-energy technology enables long operational life with minimal power consumption for applications such as mobile communications, sports and fitness, health care, security and home entertainment.

Press Materials 2012-05-29

 
N5182A and N5162A MXG ATE Vector Signal Generators - Data Sheet  
Complete N5182A and N5162A MXG ATE performance specifications are available in the data sheet.

Data Sheet 2012-05-21

MIMO Over-The-Air Research, Development, and Testing 
International Journal of Antennas and Propagation, May 2012 article provides information on the many challenges of identifying the optimal channel models and test method(s), for MIMO

Article 2012-05-09

 
Agilent Technologies Introduces 6-GHz Signal Generators with Industry-Best Performance 
Today's aerospace/defense environment requires enhanced radar performance to detect weak signals at long distances. To provide the pure and precise signals needed to test these designs, the MXG uses an innovative triple-loop synthesizer to deliver phase noise performance of -146 dBc/Hz at 1 GHz and 20 kHz offset. For developers of radar components such as mixers and analog-to-digital converters, the MXG also features industry-leading spurious performance of -96 dBc at 1 GHz.

Press Materials 2012-05-01

 
Agilent Introduces 6-GHz Signal Generators with Industry-Best Performance 

Press Materials 2012-05-01

 
Agilent Technologies Named Oscilloscope Company of the Year 
The award is based on Frost & Sullivan's recent analysis of the oscilloscope market. Frost & Sullivan ranked Agilent as the No. 2 company in 2009, but its rapid revenue growth since then has made it the leader in market penetration.

Press Materials 2012-04-25

 
N4010A Wireless Connectivity Test Set - Brochure 
The N4010A is the first test solution to deliver the ability to test Bluetooth, Bluetooth EDR, Bluetooth low energy, WLAN, and ZigBee in a single, easy-to-use, desk-top box.

Brochure 2012-03-30

PDF PDF 6.76 MB
Two-Stage Over-the-Air (OTA) Test Method for LTE MIMO Device Performance Evaluation 
International Journal of Antennas and Propagation, February, 2012, article introduces a novel, flexible, and cost-effective method for measuring MIMO OTA using a two-stage approach.

Article 2012-03-28

 
Tackling MIMO Design and Test Challenges for 802.11ac WLAN 
This article from Microwave Journal shows how the system engineer can use system simulation to help understand the design performance and design requirements needed to achieve transmitter system-level metrics such as EVM.

Article 2012-03-11

 
Using a Network and Impedance Analyzer to Evaluate 13.56 MHz RFID Tags and Readers/Writers 
For engineers who work in RFID antenna design and test, this note discusses testing RFID antenna characteristics such as impedance and resonant-frequency with network and impedance analyzers.

Application Note 2012-02-08

Testing broadband CATV amplifiers with true wideband channel rasters 
The most efficient way to measure amplifier EVM or MER is to apply a complex wideband signal generated by the M8190A and measure the resulting output with a signal analyze.

Application Note 2012-01-31

PDF PDF 456 KB
Evaluating Fluorescent Lighting Interference on Passive UHF RFID Systems - Application Note 
This paper highlights how the use of N934xC handheld spectrum analyzers are an effective way to determine if the effects of fluorescent lighting is impacting an RFID system

Application Note 2011-11-30

Learn about 3GPP LTE and other Cellular technologies with these useful resources 
Download many application notes and brochures and view videos.

Promotional Materials 2011-11-17

 
Agilent Technologies Introduces Signal Processing Libraries for 802.11ac WLAN and 60-GHz 802.11ad  
Agilent Technologies Inc. (NYSE: A) today released SystemVue 2011.10, the latest update to the leading design environment for wireless physical-layer architects.

Press Materials 2011-11-16

 
Agilent Technologies Introduces Innovative Multi-Measurement Signal Analyzer Capability for Wireless 
Agilent Technologies Inc. (NYSE:A) today announced that an innovative, new multi-measurement capability is being added to its 89600 VSA software, enabling simultaneous signal analysis of multiple carriers and signal formats for more efficient testing and deeper signal insight in wireless test.

Press Materials 2011-11-15

 
802.11ac Wireless LAN: what’s new and the impact on design and test 
EE times article by Agilent’s Mirin Lew describing the 802.11ac, the technical challenges and comparisons to earlier technologies.

Article 2011-11-09

 
Agilent Technologies' PXA Signal Analyzer Now Enables Wideband Measurement with up to 900  
Agilent Technologies Inc. (NYSE:A) today announced that its high-performance PXA signal analyzer now supports up to 900 MHz of intermediate-frequency bandwidth, enabling it to act as a broadband down converter for analysis of wideband communications and radar signals in aerospace and defense applications.

Press Materials 2011-09-20

 
Agilent Technologies Introduces Wideband DPD Modeling Platform for LTE-Advanced, 802.11ac  
Agilent Technologies Inc. (NYSE: A) today announced the newest release of its W1716 Digital Pre-Distortion Builder (DPD) software, designed to enable the high levels of wireless performance necessary for emerging wideband standards such as LTE-Advanced and IEEE 802.11ac.

Press Materials 2011-08-31

 
Digital Audio Broadcasting Receiver Testing Solutions - Demo Guide 
This document discusses the measurement configurations and procedures for DAB receiver RF performance test using Keysight instruments, according to BS EN 50248.

Demo 2011-07-27

PDF PDF 2.90 MB
89601B/BN-B7Y 802.16e OFDMA & B7S 802.16-2004 OFDM, 89600 VSA Software - Technical Overview 
This technical overview provides RF and baseband engineers the industry's most comprehensive OFDMA and OFDM PHY layer analysis tools for the IEEE-802.16 standard with Option B7Y or B7S.

Technical Overview 2011-06-11

PDF PDF 1.19 MB
MIMO Tx/Rx Test Solutions - Selection Guide 
For RF engineers working with MIMO implementations in LTE. Determine the right set of Keysight products to help validate MIMO coding and the quality of MIMO signal transmission.

Selection Guide 2011-05-31

Previous 1 2 3 4 5 6 7 8 9 10 ... Next