这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

MIMO的WiMAX实施

移动WiMAXTM是在IEEE 802.16e标准的基础上发展起来的,它正在不断克服市场限制,飞速向前发展。预计在2007年发布的第二波产品将包含MIMO(多路输入,多路输出)技术。该技术与MIMO智能天线技术连用,可以增加无线连接的数据容量并延长无线连接的距离。预计采用MIMO技术的移动WiMAX将能够承载比现有3G网络高4倍左右的通信流量,从而使无线视频变得更加可行。有关MIMO天线技术的更多信息,请查看 MIMO技术概览。

MIMO实施的独特之处是使用了OFDMA技术。在OFDMA中,用户数据猝发脉冲在时间上重叠。这最大限度地提高了复杂环境中的数据流量。

 图1.OFDMA猝发脉冲结构
 OFDMA Burst Structure

如图1中的Y轴所示,在任何一个时间点上,在不同子信道上都可获得来自多个猝发脉冲的数据。这些子信道是子载波的逻辑关系排列,而非物理关系排列。因此,相邻子载波实际上可能属于不同子信道分组,并采用不同的调制格式。虽然每个数据猝发脉冲只能是一种调制格式,但相邻子载波可以是不同的调制格式。因为每个猝发脉冲都是唯一的,所以导频将处于许多不同的子载波位置上。最终结果是,OFDM变得非常简单。

复杂性要求更深入全面的测试。是德在这个测试领域位居前列。如欲了解适用测试设备的更多信息,请参考 WiMAX测试设备。

点击下面的资料库链接,如欲查看详细的应用说明和网络技术研讨会信息,请点击下面的资料库链接。所以,当您致力于推动WiMAX和MIMO技术的创新与发展时,是德将为您排忧解难保驾护航。

”WiMAX”是 WiMAX论坛的注册商标。

资料来源:
是德网络技术研讨会(Keysight Webinars)
Wikipedia
wi-fiplanet.com

查看相关视频(优酷) 

1-25 / 51

排序:
是德科技 MIMO 接收机测试 在真实环境下精确测试 MIMO 接收机 
是德科技 MIMO 接收机测试 在真实环境下精确测试 MIMO 接收机

应用说明 2017-11-27

N5106A PXB Baseband Generator and Channel Emulator - Configuration Guide 
This configuration guide offers assistance in the ordering process for the PXB, including convenient bundles and custom configurations.

配置指南 2013-11-25

PDF PDF 1.15 MB
What every engineer needs to know about MIMO operation and measurement 
Utilizing MIMO to its fullest potential requires the engineer to have basic knowledge of its operation and measurement. This EP&T article by Agilent boils this knowledge down into 9 fundamental facts.

文章 2010-09-15

 
Solutions for MIMO RF Test and Debug 
Ensuring Quick and Accurate Four-Channel, Phase-Coherent MIMO Measurements

应用说明 2010-07-14

PDF PDF 300 KB
Agilent Technologies to Showcase Latest RF/Microwave Design and Test Products at IMS 2010 

新闻资料 2010-05-11

 
安捷伦科技公司在 IMS 2010 展会上展出最新的射频/微波设计和测试产品 

新闻资料 2010-05-11

 
配有 V2895A MIMO 同步单元的 MIMO 射频信号分析和生成测试系统以软件 
灵活的 MIMO 射频信号分析和生成系统/软件可使用MIMO 同步单元将 MIMO 就绪矢量信号发生器/分析仪配置为高达 8x8 MIMO 的任意 MIMO 配置为。

技术总览 2010-03-24

MIMO产线测试解决方案 
MIMO产线测试解决方案

应用说明 2010-01-01

N5106A PXB Baseband Generator and Channel Emulator Flyer 
Keep pace with rapid design changes using the PXB baseband generator and channel emulator to test receiver signal processing to standards and beyond.

手册 2009-12-23

PDF PDF 128 KB
推动 WiMAX 的创新和发展 
This high-level brochure focuses on Fixed and Mobile WiMAX and details Keysight's solutions along each segment of the product lifecycle.

手册 2009-12-14

PDF PDF 1.21 MB
Move Forward to What's Possible in WiMAX 
This high-level brochure focuses on Fixed and Mobile WiMAX and details Keysight's solutions along each segment of the product lifecycle.

手册 2009-12-14

PDF PDF 1.21 MB
Fading WiMAX™ testing with Keysight's E6651A and an Elektrobit Propsim C8 
This application note describes how to perform receiver testing in a faded environment with the E6651A Mobile WiMAX test set, the N6422C Wireless Test Manager software and a channel emulator

应用说明 2009-12-07

PDF PDF 788 KB
Dual Channel MIMO Measurements for WiMAX™ Wave 2 
In WiMAX Wave 2 systems, a variety of dual-channel measurements can provide essential insight into their operation and performance. Article written by Ben Zarlingo and linked with permission from Wireless Design and Development.

文章 2009-06-26

 
Understanding the Impact of Channel Effects on MIMO System Performance  
Link to article published in the March 2009 issue of Microwave Product Digest discusses unique test and measurement challenges of implementing MIMO in a wireless system

文章 2009-04-28

 
MIMO and the Battle Between LTE and WiMAX™ 
Link to April 10, 2009 Microwave Journal executive interview with Andy Botka and Carla Feldman regarding the PXB MIMO Receiver Test and the broader issue of LTE and WiMAX development.

文章 2009-04-10

 
Test solutions soup up for 4G 
Link to April 9, 2009 Microwave Journal editorial. Test equipment manufacturers are providing more capability by relying on the latest hardware and software for feature-rich and easy to use solutions with impressive raw performance.

文章 2009-04-09

 
安捷伦 MIMO/多端口连通性选件可将无线网络测试仪变成一个“多重显示(multi-up)”的 WiMAX(tm)/WLAN 移动测试解决方案 

新闻资料 2009-02-16

 
Agilent Technologies' MIMO/Multi-Port Connectivity Option Turns Wireless Networking Test Set into 'M 

新闻资料 2009-02-16

 
MIMO Measurement Tips with Keysight P-Series Power Meters and U2000 Series USB Power Sensors 
This application note provides an overview of MIMO, and shows the steps of performing an accurate and repeatable MIMO power measurement by using USB sensors or P-series power meter and sensors.

应用说明 2009-01-20

Using Base Station and MIMO Channel Emulators for Mobile WiMAX Devices 
This article describes how a channel emulator can be used to characterize the performance of a MIMO receiver. The testing was done in stages of increasing complexity, namely testing under AWGN conditions, MIMO testing with known static channels, and finally testing with channels chosen to represent “real world” behavior.

文章 2009-01-11

PDF PDF 1.37 MB
N6422C WiMAX™ Wireless Test Manager - Technical Overview 
Keysight's test manager software provides ready-to-use tests, test plans, test sequencing, and menu-selectable hardware support for quick and easy automation of device verification and pre-conformance test processes.

技术总览 2008-12-17

Agilent Technologies' Firmware Update for its Mobile WiMAX™ Test Set Enables Faster Data  

新闻资料 2008-09-25

 
Agilent Technologies' New Software Options Provide Full Drive Test Functionality  

新闻资料 2008-08-25

PDF PDF 124 Bytes
安捷伦最新软件选件可提供完整的驱动测试功能 

新闻资料 2008-08-25

PDF PDF 124 Bytes
Analyze Antenna Approaches for LTE Wireless Systems 
Multiple-antenna techniques are a large part of improved performance in LTE wireless systems, but they must be properly understood in order to be properly tested.

文章 2008-08-13

 

1 2 3 下一页