Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

WiMAX™ Implementation of MIMO

Mobile WiMAX™ is based on the IEEE 802.16e standard but is evolving in waves as it overcomes market limitations. Wave 2 products include MIMO (Multiple Input, Multiple Output) techniques. The techniques used with the smart antenna technology of MIMO makes it possible to put more data into a wireless connection and extend the range. It is expected that Mobile WiMAX with MIMO will be able to carry approximately 4x more traffic than today’s 3G networks. In this case, wireless video becomes more realistic. The unique aspect of the MIMO implementation is the use of OFDMA. In OFDMA user data bursts overlap in time. This maximizes data flow in a complex environment.

  Figure 1. OFDMA burst structure.
  OFDMA Burst Structure

At any one point in time, there is data from multiple bursts available on different subchannels, as shown on the Y axis of Figure 1. These subchannels are logical arrangements of subcarriers, not physical arrangements of subcarriers. Therefore, adjacent subcarriers may actually belong to different subchannel groupings and be different modulation formats. While each data burst may only use one modulation format, adjacent subcarriers may have different modulation formats. And because each burst is unique, the pilot locations will be at many different subcarrier locations. The end result is a complexity not found in OFDM.

The complexity drives more sophisticated testing. Keysight is on the forefront of this testing. Accelerate Wireless Design and Test with Flexible, High-Performance Platforms

Sources: Keysight Webinars, Wikipedia, wi-fiplanet.com

Посмотреть видеоматериалы на YouTube 

1-7 из 7

Упорядочить:
Move Forward to What's Possible in WiMAX 
This high-level brochure focuses on Fixed and Mobile WiMAX and details Keysight's solutions along each segment of the product lifecycle.

Брошюра 2009-12-14

PDF PDF 1.21 MB
Fading WiMAX™ testing with Keysight's E6651A and an Elektrobit Propsim C8 
This application note describes how to perform receiver testing in a faded environment with the E6651A Mobile WiMAX test set, the N6422C Wireless Test Manager software and a channel emulator

Руководство по применению 2009-12-07

PDF PDF 788 KB
Using Base Station and MIMO Channel Emulators for Mobile WiMAX Devices 
This article describes how a channel emulator can be used to characterize the performance of a MIMO receiver. The testing was done in stages of increasing complexity, namely testing under AWGN conditions, MIMO testing with known static channels, and finally testing with channels chosen to represent “real world” behavior.

Статья 2009-01-11

PDF PDF 1.37 MB
N6422C WiMAX™ Wireless Test Manager - Technical Overview 
Keysight's test manager software provides ready-to-use tests, test plans, test sequencing, and menu-selectable hardware support for quick and easy automation of device verification and pre-conformance test processes.

Обзор технических характеристик 2008-12-17

Mobile WiMAX™ Test Set Solutions Brochure 

Брошюра 2008-10-21

PDF PDF 1.67 MB
Mobile WiMAX™ PHY Layer (RF) Operation and Measurement 
This application note describes the operation and physical layer measurements of 802.16e OFDMA Mobile WiMAX devices.

Руководство по применению 2008-07-17

PDF PDF 7.84 MB
MIMO Manufacturing Solution - Application Note 
Compares two of the most popular MIMO manufacturing test methodologies, including examples to illustrate the relative merits.

Руководство по применению 2007-07-10