这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

控制与自动化

缩小范围

去除所有优化

行业/技术

按内容类型

按产品类别

1-13 / 13

排序:
构建混合测试系统,确保在两个公共开发情景中取得成功 

应用说明 2008-10-15

Using the VISA COM I/O API in .NET - Application Note 
The Microsoft .NET architecture has many features that make it an excellent environment for Test & Measurement programmers. VISA COM I/O is an update of the older VISA C API to work in and with COM technology.

应用说明 2007-03-16

PDF PDF 345 KB
将系统软件从GPIB过渡到LAN/LXI 

应用说明 2007-02-02

测试系统开发指南AN1465-4 
测试系统开发指南AN1465-4

应用说明 2006-09-01

下一代测试系统:用LXI拓展视野 

应用说明 2005-08-01

Using LAN in Test Systems: Applications (1465-14) - Application Note and Example Programs 
Topics include balancing cost, convenience and security in three common LAN scenarios: sharing instruments, remote monitoring and data acquisition, and functional test systems. Includes downloadable example programs.

应用说明 2005-04-01

 
系统开发者指南:LAN在测试系统中的使用:网络配置 

应用说明 2004-12-28

Test-System Understanding Drivers and Direct I/O (AN 1465-3) - Application Note 
This application note answers common questions about the use of drivers and direct I/O to send commands from a PC application to the test instrument.

应用说明 2004-12-21

PDF PDF 374 KB
Using SCPI and Direct I/O vs. Drivers (AN 1465-13) - Application Note 
Using SCPI and Direct I/O vs. Drivers, the fifth note in the series, outlines the relationship between input/output (I/O) software, application software and the ability to maximize instrument interchange and software reuse in present and future systems

应用说明 2004-12-13

PDF PDF 408 KB
Test-System Computer I/O Considerations (AN 1465-2) - Application Note 
The first application note in the series, Introduction to Test-System Design, covers test-system philosophy and planning and discusses how test is used in three sectors: R&D, design validation and manufacturing

应用说明 2004-12-09

PDF PDF 189 KB
Using USB in the Test and Measurement Environment (AN 1465-12) - Application Note 
Simplify test integration with USB interface. Whether you’re setting up an ad hoc system on a lab bench or designing a permanent solution for a manufacturing line, the three best choices today for connecting modern instrumentation to computers are GPIB, LAN, and USB.

应用说明 2004-11-19

PDF PDF 194 KB
System Developer Guide Using LAN in Test Systems - PC Configuration (AN 1465-11) - Application Note 
Using LAN in Test Systems: PC Configuration,the third note in the series, describes the additional capabilities required to enable communication between a PC and LAN-enabled instrumentation. This note is a companion to Application Notes 1465-9 and 1465-10.

应用说明 2004-10-19

PDF PDF 204 KB
Using LAN in Test Systems - The Basics (AN 1465-9) - Application Note 
The basic purpose of any test system is to characterize and validate the performance of electronic components, assemblies or products. The complexity of this task depends on variables such as the physical nature of the device under test (DUT), the number of tests to be performed, the number of signals to be measured and the desired time per test.

应用说明 2004-07-29

PDF PDF 270 KB