Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Радиоизмерения

Уточнить список

По Отрасли/Технологии

По типу содержания

По типу оборудования

251-275 из 556

Упорядочить:
ADS 2014 Dramatically Improves Design Productivity and Efficiency 
Agilent announces a powerful new version of Advanced Design System software, ADS 2014. Designed to dramatically improve design productivity and efficiency with new technologies and capabilities, ADS 2014 is the software's most significant ADS release to date.

Материалы для прессы 2014-02-20

 
M9018A PXIe Chassis 18-Slots, 3U, 8GB/s - Data Sheet 
This data sheet describes the capability and advantages of the M9018A PXIe Chassis.

Техническая информация 2014-02-11

Agilent Technologies Simulation and Modeling Software Selected by Nitronex for High-Power GaN Design 
Agilent announces that Nitronex, a GaAs labs company and leading producer of GaN-on-silicon RF power devices, has selected Agilent to provide a complete GaN design flow that spans both device modeling and circuit simulation.

Материалы для прессы 2014-02-11

 
On-Wafer SOLT Calibration Using 4-port PNA-L Network Analyzers - Application Note 
This documentation is intended for on-wafer applications using the 4-port, 20 GHz, PNA-L network analyzer with two dual probes to achieve full 4-port on-wafer calibrations manually. This application note provides the step-by-step instructions needed to set up a calibration kit in order to perform a 4-port SOLT (Short-Open-Load-Thru) calibration using only three thrus.

Руководство по применению 2014-02-06

Agilent Technologies’ LinkedIn ADS User Group Tops 3,000 Members 
Agilent announces that the Agilent EEsof EDA Advanced Design System (ADS) user group on LinkedIn now has over 3,000 members.

Материалы для прессы 2014-02-03

 
ADS Controlled Impedance Line Designer Solves Key Challenges in Designing Chip-to-Chip Links 
Agilent introduces Agilent EEsof EDA’s Controlled Impedance Line Designer. The software product quickly and accurately optimizes stack up and line geometry for multigigabit-per-second chip-to-chip links, using the most relevant metric.

Материалы для прессы 2014-01-27

 
GoldenGate Software Release Brings Wireless Standard-Compliant Design into RFIC Designers’ Hands 
Agilent announces the latest release of GoldenGate, its RFIC simulation, verification and analysis software.

Материалы для прессы 2014-01-06

 
Agilent Technologies Engineers Author X-Parameters* Book 
Agilent Technologies Engineers Author X-Parameters* Book

Материалы для прессы 2013-10-30

 
Agilent Technologies Announces RF and Microwave Industry-Ready Student Certification Program 
Agilent announces the RF and Microwave Industry-Ready Student Certification program, developed in conjunction with the University of South Florida, a founding partner.

Материалы для прессы 2013-10-28

 
Agilent Technologies Announces RF and Microwave Industry-Ready Student Certification Program 
Developed in conjunction with the University of South Florida, this certification program recognizes students who have demonstrated RF/MW design and measurement expertise.

Материалы для прессы 2013-10-28

 
Beyond CMOS Vs. GaAs: Picking The Right Technology 
Design software can help evaluate the many different technology options for a high-frequency electronic circuit or system under a wide range of operating conditions.

Статья 2013-10-24

 
Efficient Synthetic Aperture Radar Antenna Array Design Using Multiple Electromagnetic Solvers 
Example of a synthetic aperture radar antenna array shows how applying the most efficient EM technology to each segment of the antenna system significantly improves design efficiency compared to traditional approaches.

Статья 2013-10-11

 
UMS presents its new PDK integrating Agilent latest ADS software innovation 
United Monolithic Semiconductors (UMS) announces the availability of greatly enhanced Process Design Kits (PDKs) leveraging the latest product innovations in Advanced Design System (ADS).

Материалы для прессы 2013-10-10

 
Agilent Technologies’ Advanced Design System Selected by Kamstrup to Develop Smart Metering System 
Agilent announces that Kamstrup A/S, a provider of metering solutions for electricity, heat, water and natural gas, has selected Agilent's Advanced Design System (ADS).

Материалы для прессы 2013-10-07

 
Keysight EEsof EDA Premier Communications Design Software 
The Keysight EEsof EDA catalog provides an excellent overview of all of Keysight's Electronic Design Automation (EDA) tools.

Каталог 2013-10-07

PDF PDF 8.61 MB
N9038A MXE EMI Receiver Demo Videos on YouTube 
Explore YouTube for videos on the N9038A MXE EMI Receiver.

Демонстрация 2013-10-01

 
Agilent Technologies to Demonstrate Newest Design and Test Solutions at European Microwave Week 
Agilent announces it will demonstrate a wide range of new high-performance, flexible test solutions for designing and testing components for radar systems, antennas and next-generation wireless devices at European Microwave Week.

Материалы для прессы 2013-09-25

 
Agilent Technologies Announces Expanded Business Relationship with Gradient Design Automation 
Agilent announces a new agreement that expands its business relationship with Gradient Design Automation, a leading provider of electro-thermal simulation technology used to identify hazards and improve performance in integrated circuits that will be subject to temperature variations during operation.

Материалы для прессы 2013-08-15

 
SystemVue - System Level Design & Verification Environment - Flyer 
This flyer provides a brief description of the features and benefits provided by SystemVue - EDA software for system level design and verification.

Брошюра 2013-07-30

PDF PDF 155 KB
Industry Publications on X-Parameters 
A number if important industry publications on X-parameters.

Статья 2013-07-12

 
Microwave Journal Article: Streamlining BER Simulation and Measurement 
Bit Error Rate (BER) remains the ultimate quality metric for all communication systems. Emerging 4G systems like LTE specify throughput rate as a metric for system performance. These 4G systems add intelligence by using adaptive modulation based on channel quality, but under the hood, BER is measured while the modulation is adjusted.

Статья 2013-07-12

 
Realization and Analysis of Electronically Steerable Phased Array using Scripting & Parameterization 
With the advent of multi-core, high speed processors and abundant memory availability, complex designs using 3-D full-wave electromagnetic (EM) tools have become common choice for microwave and antenna engineers.

Статья 2013-07-09

 
Simulation and Measurement-based X-parameter Models for Power Amplifiers with Envelope Tracking 
An investigation of envelope tracking power amplifiers using simulation-based and measurement-based frequency domain static XP models.

Статья 2013-06-30

PDF PDF 544 KB
EMPro and ADS Selected by Millitech for Mixer, Multiplier and Passive Device Development 
Agilent Technologies announces that Millitech Inc., a leading provider in millimeter-wave components, assemblies and subsystems for applications in satellite communications, radiometry, radar and remote sensing, has selected Agilent’s Electromagnetic Professional (EMPro) and Advanced Design System (ADS) software for use in developing mixers, multipliers and various passive devices.

Материалы для прессы 2013-06-25

 
Active Device Characterization in Pulse Operation Using the PNA/PNA-X - Application Note 
This AN discusses pulsed S-parameter measurements using the PNA-X series and measurement techniques that enable power-dependent active device characterization including compression and distortion.

Руководство по применению 2013-06-19

Назад ... 11 12 13 14 15 16 17 18 19 20 ... Следующие