这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

射频与微波

为了满足您的大多数射频和微波测量需求,您可以在这里找到适合的应用和解决方案信息。

请务必查看一下应用指南资料库,详细了解如何使用您的设备以及如何成功完成所需的测量。

是德科技射频和数字技术学习中心――行业专家坐镇,为您的学习提供专业指导

缩小范围

行业/技术

按内容类型

按产品类别

251-275 / 572

排序:
Efficient Synthetic Aperture Radar Antenna Array Design Using Multiple Electromagnetic Solvers 
Example of a synthetic aperture radar antenna array shows how applying the most efficient EM technology to each segment of the antenna system significantly improves design efficiency compared to traditional approaches.

文章 2013-10-11

 
UMS presents its new PDK integrating Agilent latest ADS software innovation 
United Monolithic Semiconductors (UMS) announces the availability of greatly enhanced Process Design Kits (PDKs) leveraging the latest product innovations in Advanced Design System (ADS).

新闻资料 2013-10-10

 
Keysight EEsof EDA Premier Communications Design Software 
The Keysight EEsof EDA catalog provides an excellent overview of all of Keysight's Electronic Design Automation (EDA) tools.

产品目录 2013-10-07

PDF PDF 8.61 MB
Agilent Technologies’ Advanced Design System Selected by Kamstrup to Develop Smart Metering System 
Agilent announces that Kamstrup A/S, a provider of metering solutions for electricity, heat, water and natural gas, has selected Agilent's Advanced Design System (ADS).

新闻资料 2013-10-07

 
优酷-电磁兼容  
优酷-电磁兼容

基本演示 2013-10-01

 
Agilent Technologies to Demonstrate Newest Design and Test Solutions at European Microwave Week 
Agilent announces it will demonstrate a wide range of new high-performance, flexible test solutions for designing and testing components for radar systems, antennas and next-generation wireless devices at European Microwave Week.

新闻资料 2013-09-25

 
Agilent Technologies Announces Expanded Business Relationship with Gradient Design Automation 
Agilent announces a new agreement that expands its business relationship with Gradient Design Automation, a leading provider of electro-thermal simulation technology used to identify hazards and improve performance in integrated circuits that will be subject to temperature variations during operation.

新闻资料 2013-08-15

 
SystemVue - System Level Design & Verification Environment - Flyer 
This flyer provides a brief description of the features and benefits provided by SystemVue - EDA software for system level design and verification.

手册 2013-07-30

PDF PDF 155 KB
Microwave Journal Article: Streamlining BER Simulation and Measurement 
Bit Error Rate (BER) remains the ultimate quality metric for all communication systems. Emerging 4G systems like LTE specify throughput rate as a metric for system performance. These 4G systems add intelligence by using adaptive modulation based on channel quality, but under the hood, BER is measured while the modulation is adjusted.

文章 2013-07-12

 
Industry Publications on X-Parameters 
A number if important industry publications on X-parameters.

文章 2013-07-12

 
Realization and Analysis of Electronically Steerable Phased Array using Scripting & Parameterization 
With the advent of multi-core, high speed processors and abundant memory availability, complex designs using 3-D full-wave electromagnetic (EM) tools have become common choice for microwave and antenna engineers.

文章 2013-07-09

 
Simulation and Measurement-based X-parameter Models for Power Amplifiers with Envelope Tracking 
An investigation of envelope tracking power amplifiers using simulation-based and measurement-based frequency domain static XP models.

文章 2013-06-30

PDF PDF 544 KB
EMPro and ADS Selected by Millitech for Mixer, Multiplier and Passive Device Development 
Agilent Technologies announces that Millitech Inc., a leading provider in millimeter-wave components, assemblies and subsystems for applications in satellite communications, radiometry, radar and remote sensing, has selected Agilent’s Electromagnetic Professional (EMPro) and Advanced Design System (ADS) software for use in developing mixers, multipliers and various passive devices.

新闻资料 2013-06-25

 
Active Device Characterization in Pulse Operation Using the PNA/PNA-X - Application Note 
This AN discusses pulsed S-parameter measurements using the PNA-X series and measurement techniques that enable power-dependent active device characterization including compression and distortion.

应用说明 2013-06-19

Multi-Chip Module assembly in ADS2012 
Jack Sifri of Keysight Technologies demonstrates multi-chip module assembly in Keysight EEsof EDA's Advanced Design System.

基本演示 2013-06-11

 
EdXact provides new integration of Jivaro with Agilent Technologies’ GoldenGate simulator 
EdXact announces the release of a new option inside the latest version of Agilent Technologies’ GoldenGate simulator, which enables users of GoldenGate to speed up post-layout simulation suffering from an important number of parasitic netlist components.

新闻资料 2013-06-03

 
Agilent Technologies' Newest 3-D Electromagnetic Simulation Software Release Targets EMI Compliance 
Agilent announces the latest release of Electromagnetic Professional (EMPro), its 3-D electromagnetic simulation software.

新闻资料 2013-05-28

 
Agilent Technologies to Demonstrate Leading-Edge RF/MW Design and Test Solutions at IMS 
Agilent will demonstrate 25 of its newest design and measurement solutions at the IEEE MTT-S International Microwave Symposium (Booth 1230), June 2-7, at the Washington State Convention Center in Seattle.

新闻资料 2013-05-21

 
ClioSoft Announces the Integration of SOS Design Data Management with Advanced Design System 
ClioSoft's integrated solution offers ADS users seamlessly integrated revision control and enterprise design data management

新闻资料 2013-05-07

 
EM Insights Series 
The EM Insights series is a collection of EM applications from Keysight EEsof EDA.

应用说明 2013-05-06

 
Multichannel Measurements in MIMO 802.11ac Baseband IQ Simulation, Design & Test - Application Note 
This solution brief will show Keysight Technologies' complete, end-to-end solution for multichannel measurements of 802.11ac BBIQ simulation, design and test.

应用说明 2013-04-05

PDF PDF 748 KB
Agilent to Demonstrate Latest RF Circuit, System and 3-D EM Design & Simulation Solutions at WAMICON 
Agilent announces it will demonstrate its latest RF circuit, system and 3-D electromagnetic design and simulation solutions at the 14th annual IEEE Wireless and Microwave Technology Conference. WAMICON 2013 will be held April 7-9 at the Caribe Royale Hotel and Convention Center in Orlando, Fla.

新闻资料 2013-04-04

 
Enabling Simulation and Test of Custom OFDM Signals 
Orthogonal frequency division multiplexing (OFDM) has become attractive for many current and emerging commercial applications because it provides a combination of data throughput, scalability, and robustness.

文章 2013-04-01

 
Agilent Technologies Simulation Software Selected by Plextek RF Integration 
Agilent announces that Plextek RF Integration, a UK-based company that designs and develops RFICs, MMICs and microwave/millimeter-wave modules, has selected Agilent software to simulate its new high-frequency circuit and MMIC designs.

新闻资料 2013-03-27

 
A Packaged 60 GHz Low-Power Transceiver with Integrated Antennas for Short-Range Communications 
This paper describes a 60-GHz transceiver with integrated antennas for short range and low power wireless communications fabricated in a CMOS 65nm SOI technology.

文章 2013-03-25

PDF PDF 429 KB

以前 ... 11 12 13 14 15 16 17 18 19 20 ... 下一页